STM32CubeIDE (MCUs)

Ask questions on STM32CubeIDE. Discuss how to build, debug, configure, and optimize your project as well as how to use our software tools.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32CubeIDE 2.1.1 released

We are pleased to announce that the minor version 2.1.1 of STM32CubeIDE is available. What is new in 2.1.1: This release covers the topics listed below: SEGGER J-Link GDB server updated to 9.24 to fix an issue with the Live Expression view during the...

Aimen1 by ST Employee
  • 1703 Views
  • 0 replies
  • 1 kudos

STM32CubeCLT 1.21.0 released

We are pleased to announce that STM32CubeCLT 1.21.0 release is available. What is new in 1.21.0: Maintenance of the previous version: Updated in accordance with STM32CubeIDE v2.1.0Update of Clang/LLVM toolchainUpdate of GCC to GCC 14Update of STM32Cu...

Aimen1 by ST Employee
  • 638 Views
  • 0 replies
  • 0 kudos

STM32CubeIDE 2.0 release - early heads-up!

Starting from the release in November 2025, STM32CubeIDE and STM32CubeMX will be available exclusively in their standalone versions. STM32CubeMX will no longer be integrated inside STM32CubeIDE. Instead, the two tools will be interoperable in the sam...

Resolved! STM32CubeIDE compiler multiplication bug

Using:Latest STM32CubeIDENucleo-64 G071 (Cortex-M0+)GNU Tools for STM32 (9-2020-q2-update) (default)There seems to be a problem multiplying long numbers. Here's what a multiplication of two 32 bit ints looks like.And this is what a multiplication of ...

0693W000008z2cpQAA.png 0693W000008z2cuQAA.png
dscdsc by Senior
  • 1383 Views
  • 1 replies
  • 0 kudos

Copy-past project in CubeIDE failed .ioc

I want to clone my cubeIDE 1.6.1 project. But in new project .ioc file contains old name, not "CC_AVD_Second". So I can't use it.Please add .ioc renaming while project cloning.@mattias norlander​ P.S. Look also

0693W000008z202QAA.png

STM32CubeIDE 1.6.1: Cannot load examples from the network.

I have installed STM32CubeIDE 1.6.1 on a Windows 10 client. I want to load firmware examples, which I already have stored on the machine. The IDE will not connect to the network. It continually prompts me to connect to the network, but when I clic...

DMois.1 by Associate III
  • 2902 Views
  • 5 replies
  • 0 kudos

Resolved! Toolchain version control

I'm working on a project that requires very strict control of the toolchain itself. We must specify exact versions of toolchain components as part of our documentation and production process.The problem I'm having is we started work at Stm cube ide ...

Dfarr.1 by Senior
  • 2347 Views
  • 3 replies
  • 0 kudos

Resolved! A problem in Migrating from VScode to CubeIDE

Hi all, I made a project using VSCode but I need to transfer it to CubeIDE, but it is not recognized by cubeIDE so I can't open it, is there any method of migrating from VScode to CubeIDE rather than create from the beginning. Thanks

Roshan by Associate III
  • 5321 Views
  • 11 replies
  • 0 kudos

Setup application STM32F7508-DK to boot from qspi

Hi,I'm new to STM32 development board and I have an STM32F7508-DK board. I have spent days trying to have a working setup in order to have a project that makes the STM32F750 boot from the QSPI flash of the board. I have been watching youtube video an...

Renaud Dk by Associate II
  • 2581 Views
  • 3 replies
  • 0 kudos

I get an error when debugging with Cube IDE

Thank you for helping.​environment:​STM32CubeIDE Ver1.6.0​When I start debugging with the STM32Cube IDE, I get the following error:​Please tell me what to do.​Thank you.​-----STMicroelectronics ST-LINK GDB server. Version 5.8.0Copyright (c) 2020, STM...

Ebun.1 by Senior
  • 2863 Views
  • 4 replies
  • 0 kudos

Resolved! How to generate main.cpp with STM32CubeIDE

Hi, I'm working on a project in c++ and every time the IDE generates main.c instead of updating my main.cpp file. The project is set to C++, but still it generates main.c. That's very annoying. Can i fix this?

RDe R.1 by Associate
  • 4270 Views
  • 1 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.