STM32CubeIDE (MCUs)

Ask questions on STM32CubeIDE. Discuss how to build, debug, configure, and optimize your project as well as how to use our software tools.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32CubeIDE 2.1.1 released

We are pleased to announce that the minor version 2.1.1 of STM32CubeIDE is available. What is new in 2.1.1: This release covers the topics listed below: SEGGER J-Link GDB server updated to 9.24 to fix an issue with the Live Expression view during the...

Aimen1 by ST Employee
  • 1703 Views
  • 0 replies
  • 1 kudos

STM32CubeCLT 1.21.0 released

We are pleased to announce that STM32CubeCLT 1.21.0 release is available. What is new in 1.21.0: Maintenance of the previous version: Updated in accordance with STM32CubeIDE v2.1.0Update of Clang/LLVM toolchainUpdate of GCC to GCC 14Update of STM32Cu...

Aimen1 by ST Employee
  • 638 Views
  • 0 replies
  • 0 kudos

STM32CubeIDE 2.0 release - early heads-up!

Starting from the release in November 2025, STM32CubeIDE and STM32CubeMX will be available exclusively in their standalone versions. STM32CubeMX will no longer be integrated inside STM32CubeIDE. Instead, the two tools will be interoperable in the sam...

Resolved! how do i change the driver?

I'm using NUCLEO-207FZGIn cubeIDE, HAL driver is provided by default.I want to change to the SPL(Standard Peripheral Library).Since I am a beginner, I would like to get tips. Before you try, ask a question.I wonder if it is enough to simply add the S...

Psang.2 by Associate II
  • 2088 Views
  • 2 replies
  • 0 kudos

No startup script in CubeIDE?

Hi all,Have switched to the CubeIDE from Atollic. I'm curious about the absence of the startup script (the one with gdb commands) in the CubeIDE. In my project I got a bootloader at the FLASH start and before debugging in Atollic I place these gdb co...

AAlex.8 by Associate II
  • 2257 Views
  • 3 replies
  • 0 kudos

Locate Constant Data in Flash at Fixed Address

Yet another question on locating data, this time fixed in flash. I want to place some main application attributes at a fixed flash location so that my bootloader can learn about the installed app. I have had partial success. (For now this is for an S...

Grant Bt by Senior II
  • 6938 Views
  • 7 replies
  • 0 kudos

Resolved! STM32CubeIDE Update Error

Greetings!I'm trying to update my STM32CubeIDE 1.6.1 to the newest version but I get the following error:More details are here: https://pastebin.com/NpDgAkMQDoes anyone know the solution to this besides reinstalling everything?BRDomagoj

0693W00000FB1SSQA1.jpg
DTomi.1 by Senior
  • 2844 Views
  • 4 replies
  • 0 kudos

STM32CubeIDE 1.1.0 don't start on a Mac OS.

FileVault can't open check the application : "STM32CubeIDE.app is damaged and can't be open. You should placed it in garbage" (translated from french, don't sure all the world in english MacOS).Mac OS 10.14.5.I've the admin right and I can install, i...

0690X00000AsNLoQAN.jpg 0690X00000AsNLtQAN.jpg
jihzed by Associate II
  • 7078 Views
  • 14 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.