STM32CubeIDE (MCUs)

Ask questions on STM32CubeIDE. Discuss how to build, debug, configure, and optimize your project as well as how to use our software tools.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32CubeIDE 2.1.1 released

We are pleased to announce that the minor version 2.1.1 of STM32CubeIDE is available. What is new in 2.1.1: This release covers the topics listed below: SEGGER J-Link GDB server updated to 9.24 to fix an issue with the Live Expression view during the...

Aimen1 by ST Employee
  • 1703 Views
  • 0 replies
  • 1 kudos

STM32CubeCLT 1.21.0 released

We are pleased to announce that STM32CubeCLT 1.21.0 release is available. What is new in 1.21.0: Maintenance of the previous version: Updated in accordance with STM32CubeIDE v2.1.0Update of Clang/LLVM toolchainUpdate of GCC to GCC 14Update of STM32Cu...

Aimen1 by ST Employee
  • 638 Views
  • 0 replies
  • 0 kudos

STM32CubeIDE 2.0 release - early heads-up!

Starting from the release in November 2025, STM32CubeIDE and STM32CubeMX will be available exclusively in their standalone versions. STM32CubeMX will no longer be integrated inside STM32CubeIDE. Instead, the two tools will be interoperable in the sam...

Hi, I have an issue seeing the external flash loader files that I have copied into the appropriate folder, from STM32CubeIDE? Thanks, Will.

Copied my .stldr file into the directory below:-C:\Program Files\STMicroelectronics\STM32Cube\STM32CubeProgrammer\bin\ExternalLoaderbut it doesn't appear in STM32CubeIDE after I have scanned for new files in the debugger. I believe my files permissio...

WScot.1 by Associate II
  • 788 Views
  • 0 replies
  • 0 kudos

Resolved! How to add .cpp and .h files to the project of stm32cubeide?

1) I added to folder Core/Inc file my_lib.h2) Added to folder Core/Src file my_lib.cpp3) I added #include "my_lib.cpp" to main.cppIn tmy_lib.cpp I have only one class for testing. This class works with PWM. When I compile project I get errors that su...

OMaka.1 by Associate II
  • 5739 Views
  • 4 replies
  • 0 kudos

STM32CubeIDE V1.7.0, modulo arithmetic => Compiler Error?

Since 25 years I use functions or macros like #define usTimeRead() ((int16_t) (SysTick->VAL >> 1))   #define usTimePlus(TP, US) ((int16_t) TP - ((int16_t) US * (int16_t) 85))   #define usTimePast(TP) (((int16_t) TP - usTimeRead()) > (int16_t) 0)t...

ULehm.1 by Associate III
  • 12509 Views
  • 11 replies
  • 0 kudos

Resolved! CubeIDE 1.4 Hangs Using FreeRTOS

Hello everyone,I have Nucleo-L4P5ZG and the development environment is WIN10 , CubeIde1.4 and CubeMx 6.2.I am facing a strange behavior while I'm trying to debug a simple FREERTOS toggle Led code here are details:1- I started with Cube Mx and generat...

AShaban by Associate II
  • 3394 Views
  • 6 replies
  • 0 kudos

Why I can't manage embedded software packages in CubeIDE

I have downloaded and installed CubeIDE. My first question is : this is a combination of CubeMX and an IDE right? Anyway, I am trying to use Cube.AI and all tutorials talk about installing Cube.AI with CUbeMX not IDEAnyway I go to Help-> Manage embed...

STM32CubeIDE 1.7.0: No ST-LINK detected!

I know I'm not the first reporting such an issue here, but the "solutions" in the previous threads did not help.I yesterday have installed STM32CubeIDE 1.7.0 using the installer. When trying to run a code, a dialog opens saying "No ST-LINK detected!...

waldmanns by Associate II
  • 4908 Views
  • 4 replies
  • 0 kudos

Very newbe with microcontroller programming

Hello everyone!I'm start to learn MCU programming with STM32CubeIDE (have to learn by work).I've never programmed a micro before, so I'm a true beginner. I started with Youtube tutorials and learned how blink the led (by toggle, using the user button...

DMore.1 by Associate
  • 1891 Views
  • 3 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.