STM32CubeIDE (MCUs)

Ask questions on STM32CubeIDE. Discuss how to build, debug, configure, and optimize your project as well as how to use our software tools.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32CubeIDE 2.1.1 released

We are pleased to announce that the minor version 2.1.1 of STM32CubeIDE is available. What is new in 2.1.1: This release covers the topics listed below: SEGGER J-Link GDB server updated to 9.24 to fix an issue with the Live Expression view during the...

Aimen1 by ST Employee
  • 1703 Views
  • 0 replies
  • 1 kudos

STM32CubeCLT 1.21.0 released

We are pleased to announce that STM32CubeCLT 1.21.0 release is available. What is new in 1.21.0: Maintenance of the previous version: Updated in accordance with STM32CubeIDE v2.1.0Update of Clang/LLVM toolchainUpdate of GCC to GCC 14Update of STM32Cu...

Aimen1 by ST Employee
  • 638 Views
  • 0 replies
  • 0 kudos

STM32CubeIDE 2.0 release - early heads-up!

Starting from the release in November 2025, STM32CubeIDE and STM32CubeMX will be available exclusively in their standalone versions. STM32CubeMX will no longer be integrated inside STM32CubeIDE. Instead, the two tools will be interoperable in the sam...

Resolved! Problem with Running code execution and Quiting Debug using SEGGER JLink and STM32CubeIDE. Debugger requested to halt target......Target halted

Hi everybody! I am using Windows10, STM32CubeIDE v1.5.1 and SEGGER JLink debugger, HW is STM32F103C8T6, Firmware is default Blink using HAL(But its occurs in all projects)I Have 2 problems:1) Running code execution:When I try to run the code, the MCU...

AMaxs.1 by Associate II
  • 8079 Views
  • 9 replies
  • 2 kudos

Live expressions not working properly

I am atrying to look at some global variables while debugging using the live expression feature, but when I add them and run the program I can only see a blank space that some times is filled by a 0. It is like flashing sometimes, I have checked my d...

0693W00000FBjwvQAD.png
AVill.1 by Associate II
  • 1810 Views
  • 1 replies
  • 0 kudos

Division by zero

Is there a way to prevent a crash while there is a division at zero.For example when there is a division by zero it will return zero

Ecohe by Associate II
  • 7309 Views
  • 11 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.