STM32CubeIDE (MCUs)

Ask questions on STM32CubeIDE. Discuss how to build, debug, configure, and optimize your project as well as how to use our software tools.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32CubeIDE 2.1.1 released

We are pleased to announce that the minor version 2.1.1 of STM32CubeIDE is available. What is new in 2.1.1: This release covers the topics listed below: SEGGER J-Link GDB server updated to 9.24 to fix an issue with the Live Expression view during the...

Aimen1 by ST Employee
  • 1703 Views
  • 0 replies
  • 1 kudos

STM32CubeCLT 1.21.0 released

We are pleased to announce that STM32CubeCLT 1.21.0 release is available. What is new in 1.21.0: Maintenance of the previous version: Updated in accordance with STM32CubeIDE v2.1.0Update of Clang/LLVM toolchainUpdate of GCC to GCC 14Update of STM32Cu...

Aimen1 by ST Employee
  • 638 Views
  • 0 replies
  • 0 kudos

STM32CubeIDE 2.0 release - early heads-up!

Starting from the release in November 2025, STM32CubeIDE and STM32CubeMX will be available exclusively in their standalone versions. STM32CubeMX will no longer be integrated inside STM32CubeIDE. Instead, the two tools will be interoperable in the sam...

Resolved! How to see only a part of an array in expression view?

Hello!My case is:I have an array of 100 items, but now I know only the first 10 are used so I'd like to watch only the first ten variables.I know I can list the individual array items one after another (e.g, arr[0], arr[1] and so on to arr[9]), but I...

MFran.4 by Senior
  • 3785 Views
  • 4 replies
  • 0 kudos

Resolved! HAL_SAI_Start()?

With the HAL on an STM32U5 nucleo i can HAL_SAI_DMAPause() HAL_SAI_DMAResume() HAL_SAI_DMAStop() HAL_SAI_Receive_DMA() HAL_SAI_Transmit_DMA()Wouldn't it make sense to have aHAL_SAI_DMAStart()?With this nomenclature i don't have a clue how to tx/rx da...

JTedot by Associate II
  • 2063 Views
  • 2 replies
  • 0 kudos

Resolved! How to put Delay or offset Between two PWM Pulse.

Hello Members,I am new to STM32 MCUs. I am trying to generate PWM and try to modify on fly and it works. But my requirement is to have a delay between two pulse on time and it should not align to each other on any edge. Please see the photo to unders...

0693W00000JQD45QAH.jpg
Bhavik by Associate III
  • 4839 Views
  • 5 replies
  • 1 kudos

Receiving just one byte with an UART interrupt

Hi,I'm currently programming on the board F446RE with STM32CubeIDE, I'm only trying to get an array from the UART but I'm quite block.When I send an array with my computer only the first byte is sent and update in my array on the STM32. While I'm fol...

Julien33 by Associate
  • 3464 Views
  • 2 replies
  • 2 kudos

STM32Cube MCU Package vs Keil MDK packages

Hi, I am starting to use the STM32 MCUs, in specific, the STM32G0 series. I am planning to use the Keil IDE for developing. I have a question about the package that I must use. I have seen that there is to type of packages containing the CMSIS, LL an...

JNava.1 by Associate II
  • 3143 Views
  • 2 replies
  • 0 kudos

Changing from 16bit to 32bit SDRAM Problem

I am working on a project what started with a ST32F7508-DK, and I generated the code and project in TouchGFX. Everything was working fine. Then we decided to go from 16bit SDRAM to 32bit SDRAM. So we created a board that was a copy on the discovery k...

0693W00000JPXoKQAX.png
DSand.5 by Associate III
  • 5867 Views
  • 13 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.