STM32CubeIDE (MCUs)

Ask questions on STM32CubeIDE. Discuss how to build, debug, configure, and optimize your project as well as how to use our software tools.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32CubeIDE 2.1.1 released

We are pleased to announce that the minor version 2.1.1 of STM32CubeIDE is available. What is new in 2.1.1: This release covers the topics listed below: SEGGER J-Link GDB server updated to 9.24 to fix an issue with the Live Expression view during the...

Aimen1 by ST Employee
  • 1703 Views
  • 0 replies
  • 1 kudos

STM32CubeCLT 1.21.0 released

We are pleased to announce that STM32CubeCLT 1.21.0 release is available. What is new in 1.21.0: Maintenance of the previous version: Updated in accordance with STM32CubeIDE v2.1.0Update of Clang/LLVM toolchainUpdate of GCC to GCC 14Update of STM32Cu...

Aimen1 by ST Employee
  • 638 Views
  • 0 replies
  • 0 kudos

STM32CubeIDE 2.0 release - early heads-up!

Starting from the release in November 2025, STM32CubeIDE and STM32CubeMX will be available exclusively in their standalone versions. STM32CubeMX will no longer be integrated inside STM32CubeIDE. Instead, the two tools will be interoperable in the sam...

Resolved! I am new to CubeIDE and have created a c++ project. I had the system generate the code and renamed main.c to main.cpp. I then put a #include <string> in the main and I get a fatal error during the build: "string: no such file or directory."

This is running on Linux and I created a test program with the same include and compiled it with g++ without issue.I think I need to tell CudeIDE where the standard libraries are located? If that is so, Where do I find them?Thanks!!

DDurk.1 by Associate II
  • 3749 Views
  • 5 replies
  • 0 kudos

Resolved! STM32CubeIDE: using linked folders.

* This should be in MCU, Sorry * * :thinking_face:I'm trying to use a linked folder. We have several software bases that we want to use the same includes (they are all on the same hardware). On AC6 I did this by creating a linked folder. The folder o...

mreed by Associate III
  • 7281 Views
  • 7 replies
  • 0 kudos

Resolved! Using STM32cubeIDE and FreeRTOS - build Debug can't find cmsis_os.h. Release build completes with no issues.

I'm fairly new to STM32CubeIDE having used Keil uV for projects so I'm just not seeing the obvious here. No issues with build prior to enabling the FreeRTOS for NUCLEO-G474RE development target.Enable the FreeRTOS and build Release - no issues, compl...

GBrow.3 by Associate II
  • 9388 Views
  • 11 replies
  • 0 kudos

STM32F746 Timing Strangeness

I've got a Nucleo-F746 board and have noticed a code execution time anomaly that I can't explain.The code running is very simple:unsigned int j = 750000; while(j--) ;Essentially a loop that does nothing except waste time. When I run this on the ...

jerry2 by Senior
  • 5030 Views
  • 12 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.