STM32CubeIDE (MCUs)

Ask questions on STM32CubeIDE. Discuss how to build, debug, configure, and optimize your project as well as how to use our software tools.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32CubeIDE 2.1.1 released

We are pleased to announce that the minor version 2.1.1 of STM32CubeIDE is available. What is new in 2.1.1: This release covers the topics listed below: SEGGER J-Link GDB server updated to 9.24 to fix an issue with the Live Expression view during the...

Aimen1 by ST Employee
  • 1703 Views
  • 0 replies
  • 1 kudos

STM32CubeCLT 1.21.0 released

We are pleased to announce that STM32CubeCLT 1.21.0 release is available. What is new in 1.21.0: Maintenance of the previous version: Updated in accordance with STM32CubeIDE v2.1.0Update of Clang/LLVM toolchainUpdate of GCC to GCC 14Update of STM32Cu...

Aimen1 by ST Employee
  • 638 Views
  • 0 replies
  • 0 kudos

STM32CubeIDE 2.0 release - early heads-up!

Starting from the release in November 2025, STM32CubeIDE and STM32CubeMX will be available exclusively in their standalone versions. STM32CubeMX will no longer be integrated inside STM32CubeIDE. Instead, the two tools will be interoperable in the sam...

Resolved! Debug configuration for SWV Viewer is grayed out

I want to follow the video (https://www.youtube.com/watch?v=Eg_GLvLHM1o&ab_channel=STMicroelectronics) to set up the SWV Viewer, but I am not able to configure the debug configuration, as it is grayed out (like in the picture) and then also the confi...

0693W00000QLk4UQAT.png
TKleg.2 by Associate II
  • 3625 Views
  • 2 replies
  • 1 kudos

Resolved! relative and absolute paths in STM32CubeIDE

We're working on a projekt with different µC and some so called "Common-Modules".These commons are located side by side our projects and shall simply been linked to these. All this could be done, but on building the project, we noticed, that no modul...

K2R by Associate II
  • 7775 Views
  • 6 replies
  • 0 kudos

Need a working project with FreeRTOS and FATfs with CubeIDE Version: 1.10.0 and STM32CubeF4 Firmware Package V1.27.0

Hi community, Please provide me with a working example with CubeIDE Version: 1.10.0 and STM32CubeF4 Firmware Package V1.27.0 which contains both FreeRTOS and FATfs.The DMA handling seems buggy after several releases and none of the fixes mentioned in...

NSeba by Associate III
  • 1971 Views
  • 3 replies
  • 0 kudos

[resolved] Rename/Checkout STM32 Project to different folder

Sometimes I end up working on multiple branches of a project (ain't life fun!).With STM32CubeIDE it seems if I rename the project folder Project Project_Main Project_BranchXThen the Sources paths defined in the project are broken/lost, and any exclud...

Paul1 by Lead
  • 3979 Views
  • 5 replies
  • 0 kudos

Resolved! How to programming using JTAG

Hello,I am using the STM32CUBEIDE , I am working on STM32H745 series , I have to programme the device using JTAG .How I can done that which application I have to use for progrraming what setup I have to done in stm32cubeide ? Can u please help me

MDeva.1 by Associate II
  • 11689 Views
  • 3 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.