2022-07-10 10:12 AM
Hi community, Please provide me with a working example with CubeIDE Version: 1.10.0 and STM32CubeF4 Firmware Package V1.27.0 which contains both FreeRTOS and FATfs.
The DMA handling seems buggy after several releases and none of the fixes mentioned in other posts work for me.
2022-07-14 3:05 AM
Hello @NSeba and welcome to the Community :)
I suggest to refer to one of examples provided within STM32CubeF4 MCU package and get inspired from the application:
\STM32Cube_FW_F4_V1.27.0\Projects\STM324x9I_EVAL\Applications\FatFs\FatFs_uSD_RTOS
Thanks
Imen
2022-07-18 10:13 AM
Hi,
Thanks for your suggestion. the project given in the directory doesn't have an IOC file to change the controller.
2022-07-18 10:13 AM
I request somebody to give at-least an IOC file of a working project so that I can confirm the settings.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.