2023-08-24 1:11 AM
Good morning,
I apologize if this question is a bit dumb, I'm still learning embedded programming.
I'd like to know if its possible to share code between projects in STM CUBE IDE.
The idea is to have like a "folder" with one (or many) .h and .c files. Then in the properties of each project, when I need those files I just add them to the 'Paths and Symbols'.
And then wen I want to change the behavior I only change it once for all the projects.
That I already can do. The problem is that I don't know how to get that "folder" to compile. I know that compiling is a device-targeted procedure but the code in those files that I want to include won't have any reference to any specific platform.
I want to do generic code using standard libraries so it can be included in all the project's I create regardless of the micro controller.
That's why I need it to be able to "pre compile"?? without specifying a target device? Just to know whether the code is written ok.
Thank you for your help!
2023-08-24 1:24 AM
Yes, of course, in the same way as in other software. You can share source folders among several projects. You can make a static library (for compatible MCUs). You can exclude some files from build, per project configuration. By the way, CubeIDE comes with a user guide. It is written specially to answer many questions :)
2023-08-25 8:55 PM
I use a different approach.
I have one file that's unique per project (for configuration). In that file I have a lot of #define statements, which enable and disable subsystems, and customize others (like which SPI interface an SPI display uses, if enabled).
In the entire project, I use a lot of #ifdef statements.
I have one repository of all the source files. I take the root of that subdirectory (I have graphics/hardware/system, etc files), and drag and drop it into the "core" directory of the project. In the "INC" part of the core files, I include the "options.h" file.
Similar projects can use the options.h file without much editing. New projects with new features need new options in the "options.h" file. This works well over a number of projects, but you do have to be careful about what the #defines control.
In the import, make sure that you link to existing files. This allows a copy, so editing the source files changes the files for all projects. It keeps things consistent, but you have to be aware you're changing things for all the projects.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.