STM32CubeIDE (MCUs)

Ask questions on STM32CubeIDE. Discuss how to build, debug, configure, and optimize your project as well as how to use our software tools.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32CubeIDE 2.1.1 released

We are pleased to announce that the minor version 2.1.1 of STM32CubeIDE is available. What is new in 2.1.1: This release covers the topics listed below: SEGGER J-Link GDB server updated to 9.24 to fix an issue with the Live Expression view during the...

Aimen1 by ST Employee
  • 1703 Views
  • 0 replies
  • 1 kudos

STM32CubeCLT 1.21.0 released

We are pleased to announce that STM32CubeCLT 1.21.0 release is available. What is new in 1.21.0: Maintenance of the previous version: Updated in accordance with STM32CubeIDE v2.1.0Update of Clang/LLVM toolchainUpdate of GCC to GCC 14Update of STM32Cu...

Aimen1 by ST Employee
  • 638 Views
  • 0 replies
  • 0 kudos

STM32CubeIDE 2.0 release - early heads-up!

Starting from the release in November 2025, STM32CubeIDE and STM32CubeMX will be available exclusively in their standalone versions. STM32CubeMX will no longer be integrated inside STM32CubeIDE. Instead, the two tools will be interoperable in the sam...

Resolved! Inquiry about clock activation of stm32cube.

Hello?As the title states, I would like to inquire about the settings of STM32CUBEIDE(V1.13.1) of the STM32F730V8T product.If you select USB_OTG_FS (Dual/OTG, Host Only or Device only) for the relevant MCU, it will be activated in the clock, but USB_...

LSung.1 by Associate III
  • 2881 Views
  • 4 replies
  • 0 kudos

Update USB HOST library in STMcubeIDE

HiI use the USB Host library in some project with STMCUBEIDE , the processor is STM32F779AIYx.The code generator use USB host library 1.0 that have one bug at the line 561 , I must replace this line only time that update my code.I see that there is a...

PZamb.2 by Associate III
  • 2274 Views
  • 2 replies
  • 0 kudos

STM32CubeIDE v1.31.1 error when using 1.17.1 FW patch.

Hi, I have an odd error since updating to 1.17.1 FW on the STM32F7, My setup is :Board -  STM32F769I-DISCOSTM32CubeIDE - 1.13.1After updating with the FW Patch v1.17.1, my project now complains "Code Generation could not be done probably because the ...

SteveFen by Associate
  • 9464 Views
  • 6 replies
  • 1 kudos

hardfault handler

I was using stm32 cube mx to configure a pin to toggle the led so code generated using cube mx and then i just wrote the required function to toggle the led but once the code is compiled it shows zero errrors. when i debugged it and started running t...

pujitha by Associate
  • 1307 Views
  • 1 replies
  • 1 kudos

Resolved! STM32 Software is free?

Please comments whether STM32cube IDE software is free or licensed? We will use it for checksum verification, programming or re-programming.Thanks You.

SujitG by Associate
  • 5684 Views
  • 3 replies
  • 0 kudos

Resolved! HAL_TIM_PeriodElapsedCallback firing very prematurely

Hello, all.I am using STM32CubeIDE with an STM32G030 micro. I attempted to implement a simple interrupt - based timeout timer on Timer17 using the HAL driver. See attached file “Screenshot1”for the TIM7configuration info. Here’s the Init Code generat...

Resolved! CubeIDE generates redundant prototype

Today I tried migrating our projects to the new STM32CubeIDE release. One thing I noticed is that whenever MPU is enabled, it generates redundant function prototype static void MPU_Initialize(void); in main.c which generates a warning when -Wall is e...

heveskar_0-1689079501995.png heveskar_1-1689079534448.png
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.