STM32CubeIDE (MCUs)

Ask questions on STM32CubeIDE. Discuss how to build, debug, configure, and optimize your project as well as how to use our software tools.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32CubeIDE 2.1.1 released

We are pleased to announce that the minor version 2.1.1 of STM32CubeIDE is available. What is new in 2.1.1: This release covers the topics listed below: SEGGER J-Link GDB server updated to 9.24 to fix an issue with the Live Expression view during the...

Aimen1 by ST Employee
  • 1703 Views
  • 0 replies
  • 1 kudos

STM32CubeCLT 1.21.0 released

We are pleased to announce that STM32CubeCLT 1.21.0 release is available. What is new in 1.21.0: Maintenance of the previous version: Updated in accordance with STM32CubeIDE v2.1.0Update of Clang/LLVM toolchainUpdate of GCC to GCC 14Update of STM32Cu...

Aimen1 by ST Employee
  • 638 Views
  • 0 replies
  • 0 kudos

STM32CubeIDE 2.0 release - early heads-up!

Starting from the release in November 2025, STM32CubeIDE and STM32CubeMX will be available exclusively in their standalone versions. STM32CubeMX will no longer be integrated inside STM32CubeIDE. Instead, the two tools will be interoperable in the sam...

How to operate STM32 power on off

We implemented a lwip tcp server with STM32 and even sent and received messagesBut when I was debugging, it was good I'm trying to disconnect ST-LINK and see if it works by turning the power on and off without debugging, but the server didn't even cr...

ark2 by Associate III
  • 2131 Views
  • 2 replies
  • 0 kudos

Use LWIP in C++ main file

Hi every oneHow can I use LWIP TCP connection(socket, NetConn, Raw ... )  in main.cpp   ?I can use Raw in main.c properly but I need to use it in cpp files. thank you

MTora.1 by Associate III
  • 1092 Views
  • 0 replies
  • 0 kudos

STM32F4 Problem with USART

Hi, I want to use USART2 as transmitter on stm32f429zi mcu (nucleo board). I configure registers as in the picture, but transmission don't work. I use USART2 on PA2 pin and I need transmission with 115200 baudrate, alternate function is AF7 and usart...

[Debug] Software reset with bootloader

Hello everyone,on my MCU i've loaded a bootloader at address 0x0800000 and a dummy application at 0x0810000, but i'm experiencing some issues on chip reset button on the IDE. At first, when i debug the application no errors are encountered and the ap...

PGior.2 by Associate II
  • 3004 Views
  • 4 replies
  • 0 kudos

Resolved! STM32CubeIDE select target device

Hello,I have 2 NUCLEO boards connected to my computer and I don't see any option to select the target device when I run my project in STM32CubeIDE. I want to be able to run a different program on each board, how can I achieve that ?

Colus by Associate
  • 4230 Views
  • 1 replies
  • 0 kudos

TouchFX on STM32F412G not working

Hi, I am attempting to generate a simple touchgfx project then I generate the code to transfer into an STM32Cubeide project on my STM32F412G Discovery board but every time I do I just get a greyed out screen like attached image is there something I a...

Linkpad by Associate III
  • 1541 Views
  • 1 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.