2024-03-20 6:15 AM
Hi,
When I flash my code, I encounter the issue below. I have unplugged the cable of the board, but that didnt work.
Could you please help me resolve ?
STMicroelectronics ST-LINK GDB server. Version 7.5.0
Copyright (c) 2023, STMicroelectronics. All rights reserved.
Starting server with the following options:
Persistent Mode : Disabled
Logging Level : 1
Listen Port Number : 61234
Status Refresh Delay : 15s
Verbose Mode : Disabled
SWD Debug : Enabled
InitWhile : Enabled
Waiting for debugger connection...
Debugger connected
Waiting for debugger connection...
Debugger connected
Waiting for debugger connection...
-------------------------------------------------------------------
STM32CubeProgrammer v2.15.0
-------------------------------------------------------------------
Log output file: C:\Users\.....\AppData\Local\Temp\STM32CubeProgrammer_a09028.log
ST-LINK SN : 066DFF575377524867051414
ST-LINK FW : V2J43M28
Board : STM32F4DISCOVERY
Voltage : 4.08V
SWD freq : 4000 KHz
Connect mode: Under Reset
Reset mode : Hardware reset
Device ID : 0x413
Revision ID : Rev Y
Device name : STM32F405xx/F407xx/F415xx/F417xx
Flash size : 1 MBytes (default)
Device type : MCU
Device CPU : Cortex-M4
BL Version : 0x91
Memory Programming ...
Opening and parsing file: ST-LINK_GDB_server_a09028.srec
File : ST-LINK_GDB_server_a09028.srec
Size : 10.00 KB
Address : 0x08000000
Erasing memory corresponding to segment 0:
Erasing internal memory sector 0
Download in Progress:
File download complete
Time elapsed during download operation: 00:00:00.459
Verifying ...
Download verified successfully
Target is not responding, retrying...
Target is not responding, retrying...
Target is not responding, retrying...
Target is not responding, retrying...
Shutting down...
Target is not responding, retrying...
Target is not responding, retrying...
Target is not responding, retrying...
Target is not responding, retrying...
Target is not responding, retrying...
Target is not responding, retrying...
Target is not responding, retrying...
Target is not responding, retrying...
Target is not responding, retrying...
2024-03-20 9:24 AM
2024-03-20 11:10 AM
Surprisingly, everything got back to normal after I closed CUBE IDE and created new project.
Thanks for your reply.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.