STM32CubeIDE (MCUs)

Ask questions on STM32CubeIDE. Discuss how to build, debug, configure, and optimize your project as well as how to use our software tools.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32CubeIDE 2.1.1 released

We are pleased to announce that the minor version 2.1.1 of STM32CubeIDE is available. What is new in 2.1.1: This release covers the topics listed below: SEGGER J-Link GDB server updated to 9.24 to fix an issue with the Live Expression view during the...

Aimen1 by ST Employee
  • 1703 Views
  • 0 replies
  • 1 kudos

STM32CubeCLT 1.21.0 released

We are pleased to announce that STM32CubeCLT 1.21.0 release is available. What is new in 1.21.0: Maintenance of the previous version: Updated in accordance with STM32CubeIDE v2.1.0Update of Clang/LLVM toolchainUpdate of GCC to GCC 14Update of STM32Cu...

Aimen1 by ST Employee
  • 638 Views
  • 0 replies
  • 0 kudos

STM32CubeIDE 2.0 release - early heads-up!

Starting from the release in November 2025, STM32CubeIDE and STM32CubeMX will be available exclusively in their standalone versions. STM32CubeMX will no longer be integrated inside STM32CubeIDE. Instead, the two tools will be interoperable in the sam...

Resolved! STM32H723 CMSIS DSP

Hi,I'm using a NUCLEO-H723ZG and I've installed the CMSIS DSP library, but when I try to compile the code something goes wrong... May you help me to understand what do I make wrong ? Thank you, Luigi

carloV_0-1717416140680.png
carloV by Associate III
  • 2867 Views
  • 2 replies
  • 0 kudos

Resolved! Debug inline assembler code

Hi,I have a inline assembly code to implement some math, like:************************************C-Code...asm(" push {%5};"" lsl %5, 1;"" add %5, %3;"...);C-Code*******************************************************Unfortunately I`m not able to ste...

berait by Associate III
  • 3136 Views
  • 3 replies
  • 0 kudos

${project_loc} in DCT will not work

Hi,I have written 2 cmd files. The first renames the main.cpp to main.c before the code generation runs. and the second renames main.c back to main.cpp afterwards. The files are in the project path. The plan was to access them with ${project_loc}\Cpp...

padawan_0-1697619556140.png
padawan by Senior II
  • 6469 Views
  • 14 replies
  • 9 kudos

Another issue with Cube login

I got my login password rejected for no apparent reason.  I use Firefox's password manager to store the passwords.  After a few tries I realised what was happening.  When I log in it is to my.st.com, so the password manager is looking for a password ...

TJack.2 by Associate III
  • 743 Views
  • 0 replies
  • 0 kudos

Unable to update STM32CubeWB package version in project

I have a STM32WB-based project (Stm32CubeIDE 1.15.0) using the STM32CubeWB 1.17.3 version and I'm not able to update the package version to the last one (nether 1.18 nor 1.19). There is not a prompt asking me to upgrade (the typical continue or migra...

323535420-e85cb673-80c9-4e8c-b406-9120f6dfe4b0.png 323544955-dd992e73-ae5d-4ebb-99c4-bcc2b1426333.png

Analysis with SEGGER

Hi all,I building  a project using FreeRTOS, now I want to use SEGGER to analysis this project.I dowload SEGGER Application and Target Sources.and I add Folder SEGGER in my project folder .Right now, i can use SEGGER or configure anything other ?Many...

noname8888_0-1717236788826.png noname8888_1-1717236830451.png

Adding google test units to my program

Hi, I'm looking for a way to test my cpp module using google tests. It uses a RNG, CRC, and UART, and i want to add unit tests and mock tests for this module. I followed several guides but with no luck so far. I cloned google testing repository and c...

Jordalic by Associate II
  • 2168 Views
  • 1 replies
  • 0 kudos

RTC to UTC - HAL library

Hello everyone, can someone help me understand how to use the RTC and convert it to UTC using the HAL libraries, without using the time.h library?

inouee by Associate II
  • 1138 Views
  • 1 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.