STM32CubeIDE (MCUs)

Ask questions on STM32CubeIDE. Discuss how to build, debug, configure, and optimize your project as well as how to use our software tools.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32CubeIDE 2.1.1 released

We are pleased to announce that the minor version 2.1.1 of STM32CubeIDE is available. What is new in 2.1.1: This release covers the topics listed below: SEGGER J-Link GDB server updated to 9.24 to fix an issue with the Live Expression view during the...

Aimen1 by ST Employee
  • 1703 Views
  • 0 replies
  • 1 kudos

STM32CubeCLT 1.21.0 released

We are pleased to announce that STM32CubeCLT 1.21.0 release is available. What is new in 1.21.0: Maintenance of the previous version: Updated in accordance with STM32CubeIDE v2.1.0Update of Clang/LLVM toolchainUpdate of GCC to GCC 14Update of STM32Cu...

Aimen1 by ST Employee
  • 638 Views
  • 0 replies
  • 0 kudos

STM32CubeIDE 2.0 release - early heads-up!

Starting from the release in November 2025, STM32CubeIDE and STM32CubeMX will be available exclusively in their standalone versions. STM32CubeMX will no longer be integrated inside STM32CubeIDE. Instead, the two tools will be interoperable in the sam...

Resolved! Can't work on CubeIDE, but can work on MDK

I want to use ThreadX and a Command-Line called letter-shell with CubeIDE, used a uart lib(lwrb) but changed it to HAL, but it will crash when send an costum command. Send string is "func 123 "hello word"".Here are a few of the ways I've tried: First...

SourFish_0-1723475584804.png SourFish_2-1723476204199.png
SourFish by Associate II
  • 3287 Views
  • 6 replies
  • 1 kudos

STM32CubeIDE and Segger j-link connection issue

Mr./Ms. Forum,I have the following system components:STM32CubeIDE Version 1.11.0Segger j-link PLUS Compact debug probe Version 11.0target hardware - custom pcb with an STM32U585CIT6 microcontrollerI can't load code into my target hardware. I have inc...

JimEno_2-1722604869490.png JimEno_0-1722604773569.png JimEno_1-1722604816308.png
JimEno by Associate III
  • 2305 Views
  • 1 replies
  • 1 kudos

Porting Threadx on STM32L496

https://github.com/eclipse-threadx/threadx/tree/master/test/tx/regression ........from that link i want to try running one of the test cases from the repo. I have STM32L496zg-p board and stm32cube IDEI need to manually port from the this repo https:/...

Resolved! NUCLEO-L4R5ZI is not connecting to STM32CubeIde

Hi,I have been trying to program NUCLEO-L4R5ZI but the ST-Link doesnt seem to be connecting. I have been going through the forums and it seems the ST-Link drivers dont work with Windows 11. Is that correct?Thank you.

arbio13 by Associate
  • 1169 Views
  • 1 replies
  • 0 kudos

Export project do not include header files

Hi everyone,I'm new to the community and I need help to export one of the example project.It seems that all the header files are not included in the zip exported.I'm wondering if I should use a different method. Any help much appreciated David

carlacda by Associate
  • 1463 Views
  • 1 replies
  • 0 kudos

STM32cubeide

Hi friends,I am built one custom made PCB with by using STM32F103C8T6 IC for my project purpose.But ,When i am trying to upload my source code by using stm32Cubeide it shows below error.Error in final launch sequence: Failed to execute MI command:tar...

Vignesh_V by Associate II
  • 2841 Views
  • 3 replies
  • 1 kudos

While compiling Code for STM32L073RZT6 getting Warning

While compiling Code for STM32L073RZT6 getting Warning :  C:/ST/STM32CubeIDE_1.7.0/STM32CubeIDE/plugins/com.st.stm32cube.ide.mcu.externaltools.gnu-tools-for-stm32.12.3.rel1.win32_1.0.100.202403111256/tools/bin/../lib/gcc/arm-none-eabi/12.3.1/../../.....

Screenshot 2024-07-08 114826.png
Mohsin by Associate II
  • 1909 Views
  • 2 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.