STM32CubeIDE (MCUs)

Ask questions on STM32CubeIDE. Discuss how to build, debug, configure, and optimize your project as well as how to use our software tools.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32CubeIDE 2.1.1 released

We are pleased to announce that the minor version 2.1.1 of STM32CubeIDE is available. What is new in 2.1.1: This release covers the topics listed below: SEGGER J-Link GDB server updated to 9.24 to fix an issue with the Live Expression view during the...

Aimen1 by ST Employee
  • 1703 Views
  • 0 replies
  • 1 kudos

STM32CubeCLT 1.21.0 released

We are pleased to announce that STM32CubeCLT 1.21.0 release is available. What is new in 1.21.0: Maintenance of the previous version: Updated in accordance with STM32CubeIDE v2.1.0Update of Clang/LLVM toolchainUpdate of GCC to GCC 14Update of STM32Cu...

Aimen1 by ST Employee
  • 638 Views
  • 0 replies
  • 0 kudos

STM32CubeIDE 2.0 release - early heads-up!

Starting from the release in November 2025, STM32CubeIDE and STM32CubeMX will be available exclusively in their standalone versions. STM32CubeMX will no longer be integrated inside STM32CubeIDE. Instead, the two tools will be interoperable in the sam...

Resolved! Slow down SAI Audio output

 Hello,I am currently programming an STM32F469I in STM32CubeIDE (I am a beginner with STM) and I am facing some issues.What I want: I want to read WAV file data from an SD card and send it to the AUX output so I can hear it on my headset/speaker. Cur...

LCKR register useage

Hi ,I am using the stm32f411VET MC board, now i implemented the code to check how LCKR register work. This is the code which i implemented for that, but when i debugged it the LCKR register bits has not set. Any one can help me. /** interfacing LED w...

suhel by Associate
  • 600 Views
  • 0 replies
  • 0 kudos

Resolved! LIve Exressions says " Failed to evaluate expressions.".

Hi.I am developing on STM32CubeIDE with F446RE Nucleo, and I want to get the voltage value by calculating ADC value.But that doesn't work.Here is the "main.c".I made two variables.(" ADC " means ADC value, " v " means voltage value.)Red texts are tex...

MED2972 by Associate III
  • 9439 Views
  • 14 replies
  • 8 kudos

debug SFRs

I can't read/change the SFR values while debugging in CubeIDE .value of all Registers is "error reading value"If I try to do that IDE throughs and error.The only way to read/change values is by suspending the debugging session.I remember this feature...

Screenshot 2024-11-14 133954.png 0693W00000NqiAGQAZ.png

Resolved! PWM on PA8 for a stm32f103rct6 does not work

I am trying to use pin PA8 as a PWM output using timer 1 on channel 1 for a stm32f103rct6. I have successfully programmed pins PA9, PA10, and PA11 to provide PWM output on channels 2, 3, and 4, but when I do the same for PA8 on channel 1, I do not ge...

JGaby.1 by Associate III
  • 2745 Views
  • 4 replies
  • 0 kudos

Resolved! ST, Please stop login strategy in your tools

Hi STI generally appreciate your tools and how to keep on make them better, keeping also quality on track.But let me say this: It is highly annoying that it is mandatory to login in the CubeMX and CubeIDE.Please remove this again.Use case: as a embed...

Led by Senior
  • 4283 Views
  • 9 replies
  • 7 kudos

error: undefined reference to 'main'

Hello!I built a CubeMX project from Simulink after I connected an STM32 H753ZI hardware to my laptop.It is giving me an error in "bl main" : C:/Users/detec/OneDrive/Documents/MATLAB/lastcon/STM32CubeIDE/Debug/../Application/User/Startup/startup_stm32...

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.