STM32CubeIDE (MCUs)

Ask questions on STM32CubeIDE. Discuss how to build, debug, configure, and optimize your project as well as how to use our software tools.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32CubeIDE 2.1.1 released

We are pleased to announce that the minor version 2.1.1 of STM32CubeIDE is available. What is new in 2.1.1: This release covers the topics listed below: SEGGER J-Link GDB server updated to 9.24 to fix an issue with the Live Expression view during the...

Aimen1 by ST Employee
  • 1703 Views
  • 0 replies
  • 1 kudos

STM32CubeCLT 1.21.0 released

We are pleased to announce that STM32CubeCLT 1.21.0 release is available. What is new in 1.21.0: Maintenance of the previous version: Updated in accordance with STM32CubeIDE v2.1.0Update of Clang/LLVM toolchainUpdate of GCC to GCC 14Update of STM32Cu...

Aimen1 by ST Employee
  • 638 Views
  • 0 replies
  • 0 kudos

STM32CubeIDE 2.0 release - early heads-up!

Starting from the release in November 2025, STM32CubeIDE and STM32CubeMX will be available exclusively in their standalone versions. STM32CubeMX will no longer be integrated inside STM32CubeIDE. Instead, the two tools will be interoperable in the sam...

Resolved! No ETH Connectivity Option for STM32F779

I cannot find the ETH connectivity option in the Pinout & Configuration window. It is listed as an option in the datasheet, and pins are given for the various MII options. What can I do to configure the MCU with a RMII interface to an external PHY ch...

jcGTRI_0-1740070191837.png jcGTRI_1-1740070353410.png
jcGTRI by Associate
  • 1381 Views
  • 3 replies
  • 1 kudos

Resolved! if-block brace ignored...why?

Hi guysIn the picture, you can see a code fragment in debugging mode. You also may see, that the controller is forced to stop at line 476, the if statement.Now the problem: I want to enter the if-branch, if the function returns with the READY typedef...

White_Fox by Associate III
  • 2889 Views
  • 4 replies
  • 1 kudos

STM32CubeIDE .cproject vs CMake files

Hello,I've started working with CMake in STM32CubeIDE: STM32CubeIDE Version: 1.17.0 Build: 23558_20241125_2245 (UTC) (C) 2024 STMicroelectronics ALL RIGHTS RESERVED Everything works perfectly, and I can compile without any issues.However, I'm not s...

Source Format function bug?

HelloI setup the IDE with the code format that I wanted under project preferences. Then I right click on the source code (*.c .h or dir), then get the context menu and select "Source"->"format.  This seems to reformat the code  as expected, but shoul...

matt-crc by Senior III
  • 1690 Views
  • 4 replies
  • 0 kudos

Changing CubeIDE Comment Color

Hi,I'm using STM32CubeIDE with the Dark theme and Default colors and fonts, and I can barely read the comments with the gray on gray color scheme (pictured below).  How can I change the color of the commented/inactive code sections?  I've gone throug...

Screenshot 2024-06-19 120600.png
hypoxic by Associate II
  • 5176 Views
  • 3 replies
  • 6 kudos

Resolved! RE: Cannot connect to STM32 target to erase memory

Hello!New to the STM controllers, failed to realize that PA13 was necessary to connect the debugger and was quite dismayed to realize my mistake after looking to program it as a GPIO. I have tried connecting with the IDE and Programmer alike, both wi...

nc_dummy_0-1739921936807.png
nc_dummy by Associate II
  • 1634 Views
  • 3 replies
  • 0 kudos

Resolved! i can't log in myST

This is the first time I use STM32cubeIDE ver 1.15.1 . While using it, there are a few operations that need to be logged in. I already have an account in the practice room at school, but when I log in on my personal laptop, I see a box. "Authenticati...

Screenshot 2024-05-14 171838.png
dnht by Associate
  • 11225 Views
  • 14 replies
  • 12 kudos

Resolved! elf has a LOAD segment with RWX permissions w/ Optimization

I upgraded my MacBook computer and installed the latest STM32CubeIDE 1.17 like many other people reporting the new warning that has appeared with the 12.3 toolchain.  I have an STM32F413 project I have been working on for a few years which uses an RT...

tlsvd by Associate II
  • 3082 Views
  • 5 replies
  • 3 kudos

STM32Cube IDE problem flashing the code

Hi, I'm able to build the project and generate the hex file. Out of sudden i'm not able to flash my board using STLink v2 neither i'm able to enter into debugging mode. Using STM32CubeProgrammer i'm able to flash the board but i want to enter into de...

ape07_0-1739940858190.png
ape07 by Associate
  • 1272 Views
  • 2 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.