STM32CubeIDE (MCUs)

Ask questions on STM32CubeIDE. Discuss how to build, debug, configure, and optimize your project as well as how to use our software tools.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32CubeIDE 2.1.1 released

We are pleased to announce that the minor version 2.1.1 of STM32CubeIDE is available. What is new in 2.1.1: This release covers the topics listed below: SEGGER J-Link GDB server updated to 9.24 to fix an issue with the Live Expression view during the...

Aimen1 by ST Employee
  • 1703 Views
  • 0 replies
  • 1 kudos

STM32CubeCLT 1.21.0 released

We are pleased to announce that STM32CubeCLT 1.21.0 release is available. What is new in 1.21.0: Maintenance of the previous version: Updated in accordance with STM32CubeIDE v2.1.0Update of Clang/LLVM toolchainUpdate of GCC to GCC 14Update of STM32Cu...

Aimen1 by ST Employee
  • 638 Views
  • 0 replies
  • 0 kudos

STM32CubeIDE 2.0 release - early heads-up!

Starting from the release in November 2025, STM32CubeIDE and STM32CubeMX will be available exclusively in their standalone versions. STM32CubeMX will no longer be integrated inside STM32CubeIDE. Instead, the two tools will be interoperable in the sam...

Resolved! ADC1_IN16 uasge

Hi,I am using the latest version v1.16.0 STM32CubeIDE with stm32g071cb.It is not possible to use ADC1_IN16 (PB12). I have created also a new project  to test this condition.Changing the sequencer disables IN16 or makes error condition.I need PA2 -PA3...

istepne_1-1721201408556.png
istepne by Associate III
  • 2354 Views
  • 4 replies
  • 1 kudos

Resolved! Build Analyzer with CMake toolchain

Can anyone confirm that the Build Analyzer in the CubeIDE works when using the CMake toolchain? For compatibility reasons I'm currently stuck at IDE version 1.16.1. I created a fresh CMake Project for a Nucleo board (U545). It creates the elf and map...

stryga by Associate III
  • 1504 Views
  • 2 replies
  • 0 kudos

Resolved! Capturing SWV data stream from GDB

I've got SWV output showing within the STM32CubeIDE. I would now like to be able to capture this output from the command line using gdb. Is there any documentation on how to activate the SWV in gdb?I've tried using: monitor swo enable 4500000 decode ...

CTapp.1 by Senior III
  • 1199 Views
  • 1 replies
  • 0 kudos

Resolved! Graphics change on the display through the code

Hello guys can someone please help me change the graphic on the display through the code? My boss sent me a video in French, which I don't understand at all. I've already Googled and searched but haven't found anything yet. I'm using the STM32746G-Di...

Bea_12 by Associate III
  • 1196 Views
  • 2 replies
  • 2 kudos

Disable Helium extension using STM32 cube ide

Hi all,I am using the STM32N6570-DK kit with the GCC compiler. I want to disable the Helium extension. I have taken the AI object_detection code as a base code and created one function to check whether the Helium extension is enabled or disabled. I r...

VasuV by Associate II
  • 2292 Views
  • 3 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.