STM32CubeIDE (MCUs)

Ask questions on STM32CubeIDE. Discuss how to build, debug, configure, and optimize your project as well as how to use our software tools.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32CubeIDE 2.1.1 released

We are pleased to announce that the minor version 2.1.1 of STM32CubeIDE is available. What is new in 2.1.1: This release covers the topics listed below: SEGGER J-Link GDB server updated to 9.24 to fix an issue with the Live Expression view during the...

Aimen1 by ST Employee
  • 1703 Views
  • 0 replies
  • 1 kudos

STM32CubeCLT 1.21.0 released

We are pleased to announce that STM32CubeCLT 1.21.0 release is available. What is new in 1.21.0: Maintenance of the previous version: Updated in accordance with STM32CubeIDE v2.1.0Update of Clang/LLVM toolchainUpdate of GCC to GCC 14Update of STM32Cu...

Aimen1 by ST Employee
  • 638 Views
  • 0 replies
  • 0 kudos

STM32CubeIDE 2.0 release - early heads-up!

Starting from the release in November 2025, STM32CubeIDE and STM32CubeMX will be available exclusively in their standalone versions. STM32CubeMX will no longer be integrated inside STM32CubeIDE. Instead, the two tools will be interoperable in the sam...

Resolved! stm32u5 OpenOCD and stlink-server issues on macOS

I am trying to connect to the b-u585i-iot02a on macOS 15.3.1 using OpenOCD without success. The same board, cables and configuration scripts with the same version of OpenOCD (0.12.0+dev-01888-ga168c6341) works on both Windows 11 and Ubuntu 24.04. ST-...

larschrj by Associate
  • 2255 Views
  • 2 replies
  • 2 kudos

Resolved! Incorrect path .elf file

Recently I changed from Windows to Linux. Now I'm working on a older project and when debugging I got the message "program file does not exist" wit the details:.../Projects/VxxT/VxxT_firmware/Debug\VxxT.elf not foundI've found that the problem is the...

freddy by Associate II
  • 1734 Views
  • 4 replies
  • 6 kudos

STM32CubeIDE 1.18 not work -u _printf_float

 char stringUSBCDC[50]; sprintf(stringUSBCDC, "Hello v%f\n", 1.0f); while (1) { CDC_Transmit_FS((uint8_t*)stringUSBCDC, strlen(stringUSBCDC)); In terminal - outputHello vHello vHello vHello vCode formatting applied - please see How to insert sourc...

Alex2670 by Associate II
  • 2273 Views
  • 6 replies
  • 1 kudos

STM32H7B3I-DK - Getting the SWV ITM To work

Hi, I noticed a few people were having problems getting the SWV Console to work.  I had the same trouble with the STM32H7B3I-DK. Trace would work, but neither the ITM or the Profiler would produce anything.  I fixed it by making the clock frequency s...

2025-03-08_17-31-52.png

Resolved! Linker Warnings on every new project

Moved from MPUs forumEvery new project I start now has linker error at the endD:/STMicro/STM32Cube/IDE_1.14/STM32CubeIDE/plugins/com.st.stm32cube.ide.mcu.externaltools.gnu-tools-for-stm32.11.3.rel1.win32_1.1.100.202309141235/tools/bin/../lib/gcc/arm-...

CubeIDE V1.18.0 Does not link project correctly

Hi, I have a touchGFX V4.23.2 project  written with CubeIDE at least four IDE versions ago and have not had any upgrade problems until I upgraded from 1.17.0 to 1.18.0. When I do a clean build I end up with memory link assignment errors: When I do a ...

Snag_24f16061.png Snag_24f24b0f.png

STM32 Uart and PWM doesn't work at the same time

Hello, I have urgent work. In the code I have, pwm is written as bare metal and uart is written with hal. I am using the STM32 F401RE model. PWM uses TIM1 CH1 and Ch2, TIM 10, TIM11, and Uart is with the TIM 2 Hal library. When I run the code alone, ...

Maprex by Associate II
  • 1466 Views
  • 1 replies
  • 0 kudos

Resolved! Debug - watch variable error

I'm trying to debug my UART debug code. I suspect that I have calculated the Baud rate incorrectly.I run the code in debug & I'm trying to view the value in `what_baud` but the debugger isn't having it, see below.How do I do this correctly? 

NicRoberts_0-1744210631725.png
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.