2023-09-08 2:14 PM
Hello again,
After configuring all of the peripherals and pins, I have run into another problem. I need to enable the Azure RTOS but I don't have any selection for U5. I am on the latest build now and I downloaded the latest FW package (1.3.0). I'm using the STM32U599VJT6.
I see others talking about using it and there are videos about it so I must be doing it wrong. Is there a package that I am not seeing is missing? I am using Azure for an H7 project but it was a while ago so maybe I'm just missing something with this new chip!
Thanks so much!
Michael
Solved! Go to Solution.
2023-09-08 2:56 PM - edited 2023-09-08 2:57 PM
2023-09-08 2:56 PM - edited 2023-09-08 2:57 PM
2023-09-08 3:14 PM
Thank you again for the continued fast support! I guess it really was different with the H7. I won't pretend to be an expert with each change and so perhaps this is just adding the ThreadX option from the "middleware and software packs" selections. I'm going to keep digging into this and would like to leave this discussion open, in case I have more questions on this, if that is okay.
Thanks again!
Michael
2023-09-08 3:20 PM
Hello again @MichaelW
I will be always happy to help if i can. But i Suggest you to close this topic by choosing a best answer and than ask your next questions in a new post to give them more visibility and more people can give help.
Best regards.
II
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.