2023-02-07 4:37 AM
#define VBLOCKENTRIES 22
int16_t indexVDial = 0, ixVBFree = 0;
int16_t blocksSet[2][VBLOCKENTRIES][4];
blocksSet[indexVDial][ixVBFree][1] = 0x1000; / Fails to write to array
2023-02-07 7:50 AM
May depend on the index values which are not shown in your code sample.
Anyway, 123123 is not an int16_t
hth
KnarfB
2023-02-07 8:04 AM
Hard to know dimensions / size here, or index values. Could get quite large, probably would avoid as a local/auto variable.
Provide more context.
2023-02-07 10:11 AM
Index values given, it isn't addressing the memory correctly, so I was wondering if there is an issue with 3 dimensional arrays?
2023-02-07 10:14 AM
True, it's reasonably small though int16_t[2][22][4], around 350 bytes.
It just doesn't write or read the values, I could manually set them in debug, but it was as if it just ignored the C code. Looking at the asm it looked too short to index correctly, just wondered if there was a known limitation with arrays with over 2 dimensions.
2023-02-07 10:17 AM
Never heard of such a limitation. Is the result used in the code? Could the assigment be optimized away?
2023-02-08 12:23 AM
Yes it's used, I change from a 3D array to two 2D arrays, using the same indices, and it works correctly. [Table 0/1][Entry 0-21][0-4 int16 data] just fails to work at all. Weirdly in debug I can hover the cursor over the code line to set a value, and set it in the pop-up window, but it ignores the code line being executed:
entries[0][0][0] = 123; and nothing is written to the first table, first entry first int16
2023-02-08 12:30 AM
Odd, perhaps there's a bug in the GNU/GCC compiler.
Look at the assembler generated at different optimization settings.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.