2024-11-19 6:35 AM - edited 2024-11-19 8:06 AM
Hello,
my injected Adc sequence was not being triggered, and I found that the cause is that, with LL driver, the trigger source is not being set by the CubeMX code generation.
I had to add this line in the main code:
LL_ADC_INJ_SetTriggerSource(ADC1,LL_ADC_INJ_TRIG_EXT_TIM1_CH4);
I am testing on a Nucleo L432KC
P.S. I have fitted SB17 to have the 8MHz clock in from the STLInk. Otherwise, to use a default solder bridge configuration, the clock source in the IOC file needs to change.
Solved! Go to Solution.
2024-11-20 4:02 AM
Hello @MD ,
The issue is confirmed, and it will be investigated by the STM32cubeMX team (Internal ticket number: 196636),
Thanks.
Mahmoud
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2024-11-19 7:16 AM
Hello @MD ,
First let me thank you for posting.
Your request is under investigation. I will get back to you ASAP.
Thanks.
Mahmoud
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2024-11-20 4:02 AM
Hello @MD ,
The issue is confirmed, and it will be investigated by the STM32cubeMX team (Internal ticket number: 196636),
Thanks.
Mahmoud
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.