2026-03-04 4:13 AM
Hello,
In a paused debugging session, in the Run and Debug > Variables > Local list, if I right-click the varaible, the context menu has an item "Show in Memory Inspector".
Clicking it opens the Memory Inspector, but with the name of the variable as the adress ( &(pRxData) for example), which the memory viewer cannot resolve into the actual address (0x20003DC0 for example).
For this functionality to be most useful, I would expect either the Memory Inspector to be able to resolve the variable, or the command to open the Memory Inspector with the already-resolved address.
Best regards,
Nicolas
2026-03-04 11:39 PM - edited 2026-03-05 12:07 AM
I see the issue also, but only with some local stack based variables. Global and static variables work fine.
Using vscode with STM32Cube extensions v3.7.0, STLINK-V3MINIE and STM32N65x0 MCU. GCC compiler and -O2 optimization.
2026-03-05 12:56 AM
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.