2023-07-01 1:51 AM
I want to develop a host computer software based on the st-link library and use C++ to implement the flush function of reading and writing, how can I get this st-link library and API usage?
2023-07-01 3:18 AM
what is this " st-link library" ? explain, what you expect to do.
and what "implement the flush function" for ? give example, how it should work.
2023-07-01 3:52 AM
I saw that Segger has the j-link SDK to develop host computer software for users to erase and write FLASH. My application environment is: the host computer is connected to the MCU through the st-link v2 emulator, and then use the software I developed to read and write the FLASH of the mcu, I see on the Internet that your company also has a similar j-link sdk, do I want to develop such a software is there a similar SDK?Or how can it be achieved?
2023-07-01 4:09 AM
a. its not MY company, i just use the cpu...and other.
b. so using st-linkv2 you want make a program like stm32CubeProgrammer ? that is possible, look for the app note about it.
2023-07-01 6:56 AM
Yes, I want to make a simple software like this stm32CubeProgrammer, But only need to read or write the content of a specific address in MCU's FLASH."
2023-07-01 8:17 AM
Perhaps something like https://github.com/stlink-org/stlink
2023-07-01 6:20 PM
thanks!
2023-07-02 12:10 AM
The CubeProgrammer API docum and examples is installed with the CubeProgrammer. YMMV.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.