2025-12-14 8:59 AM - edited 2025-12-14 9:08 AM
Hello,
I am trying to generate a STM32CubeIDE project using CubeMX (version 6.16.1) for MP157D-DK1 board. It generates some device trees (linux, u-boot, tp-a) but it fails to generate the CubeIDE project.
I also tried older versions of CubeMX (as late as 6.12) and none work.
The error it displays is attached. Any idea what might be going wrong with the code/project generation? I have STM32CubeIDE v2.0.0 installed.
Thanks.
Solved! Go to Solution.
2025-12-14 9:13 AM
2025-12-14 9:13 AM
2025-12-14 9:46 AM
Allright, it seems that setting the hostname to "localhost" fixes the problem. I am also using openSUSE (Tumbleweed). Thanks.
2025-12-14 10:17 AM
Since this seems like a bug that is now over 3 years old and the workaround is working on openSUSE,I'll perhaps also try using Ubuntu/Fedora distrobox container for my STM tools to avoid further problems for the time being.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.