2020-06-22 2:03 AM - last edited on 2023-07-12 10:13 AM by Kevin HUBER
There are only a linux path suggested, no windows path. If windows is not supported, then it is not stated in previous steps. If it is supported, then path is missing at step 2.1
/Peter
2020-06-22 4:48 AM
Hi @PLied,
The MP1 Cube itself can also be used on Windows - for development of M4 core code.
But because most of development is running on Linux only the recommended path is for Linux.
See: https://wiki.st.com/stm32mpu/wiki/PC_prerequisites
So in windows you can place this package anywhere according your needs.
Best regards,
Milan
2020-07-01 7:05 AM
Well, I have been using IAR for decades and Cortex-M for quite some time so I will stick to what I am used to, Windows host for development. I prefer to use linux as virtual machines without desktop and use filesharing with windows where needed. Don't assume that there are only Linux desktops used by developers...
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.