2024-12-08 1:52 PM
Hi,
I have to use OpenStLinux 3.0 Developer SDK for my project.
I am using stm32cubemx 6.3.0 to generate the project files.
I then use Stm32cubeide 1.16.1 to import the project.
I was able to specify the location of the installed Developer SDK package 3.0.
However, when I proceed to install the OpenStLinux 3.0 source codes plugin, the IDE will just crush!!!!
Just to confirm, I read on the wiki that Stm32cubeIDE 1.16.1 will import and support Developer SDK package 3.0.
Anyone can help?
Thanks
2024-12-09 12:35 AM
Hi @squek
CubeIDE 1.16.1 is provided as part of what we call Ecosystem V5.
STM32 MPU ecosystem release note - stm32mpu-ecosystem-v5
What do you call "Developer SDK package 3.0" ?
Olivier
2024-12-09 1:13 AM
HI Olivier,
Thanks a lot for your swift response. Please pardon my limitations in this subject. Sorry for call stm32mpu-ecosystem-v3 as Developer SDK package 3.0. Will this Stm32CubeIDE 1.16.1 provide back compatibility to older ecoysystem such as v3?
Thanks a lot.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.