2026-01-23 5:49 AM
Hi everyone,
I'm trying to install the EGit plug‑in on STM32CubeIDE version 1.14.1, but I'm running into persistent issues.
During the installation, the dependency calculation phase fails, and CubeIDE proposes alternative solutions. If I continue using the option to keep the original installation and modify only the required components, the process eventually ends with an installation error.
The exact same problem also occurs on STM32CubeIDE version 2.0.0, so it doesn’t seem related to a single release.
Below is the full error log I receive:
An error occurred while collecting items to be installed
session context was:(profile=STM32CubeIDE,
phase=org.eclipse.equinox.internal.p2.engine.phases.Collect, operand=, action=).
No repository found containing: osgi.bundle,javax.annotation,1.3.5.v20230504-0748
No repository found containing: osgi.bundle,org.eclipse.emf.common,2.29.0.v20230916-0637
No repository found containing: osgi.bundle,org.eclipse.emf.ecore.xmi,2.36.0.v20231002-1156
No repository found containing: osgi.bundle,org.eclipse.jdt.core.compiler.batch,3.39.0.v20240820-0604
No repository found containing: osgi.bundle,com.jcraft.jsch,0.1.55.v20190404-1902
No repository found containing: osgi.bundle,com.jcraft.jzlib,1.1.1.v201205102305
No repository found containing: osgi.bundle,javaewah,1.1.6.v20160919-1400
No repository found containing: osgi.bundle,net.i2p.crypto.eddsa,0.3.0.v20181102-1323
No repository found containing: osgi.bundle,org.apache.commons.compress,1.18.0.v20181121-2221
No repository found containing: osgi.bundle,org.apache.log4j,1.2.15.v201012070815
No repository found containing: osgi.bundle,org.apache.sshd.osgi,2.2.0.v20190425-2127
No repository found containing: osgi.bundle,org.apache.sshd.sftp,2.2.0.v20190425-2127
No repository found containing: osgi.bundle,org.bouncycastle.bcpg,1.61.0.v20190602-1335
No repository found containing: osgi.bundle,org.bouncycastle.bcpkix,1.61.0.v20190602-1335
No repository found containing: osgi.bundle,org.bouncycastle.bcprov,1.61.0.v20190602-1335
No repository found containing: osgi.bundle,org.eclipse.egit,5.5.0.201909110433-r
No repository found containing: osgi.bundle,org.eclipse.egit.core,5.5.0.201909110433-r
No repository found containing: osgi.bundle,org.eclipse.egit.doc,5.5.0.201909110433-r
No repository found containing: org.eclipse.update.feature,org.eclipse.egit,5.5.0.201909110433-r
No repository found containing: osgi.bundle,org.eclipse.egit.ui,5.5.0.201909110433-r
No repository found containing: org.eclipse.update.feature,org.eclipse.emf.common,2.30.0.v20230916-0637
No repository found containing: org.eclipse.update.feature,org.eclipse.emf.ecore,2.36.0.v20231002-1156
No repository found containing: osgi.bundle,org.eclipse.jgit,5.5.0.201909110433-r
No repository found containing: osgi.bundle,org.eclipse.jgit.archive,5.5.0.201909110433-r
No repository found containing: org.eclipse.update.feature,org.eclipse.jgit,5.5.0.201909110433-r
No repository found containing: osgi.bundle,org.eclipse.jgit.ssh.apache,5.5.0.201909110433-r
No repository found containing: org.eclipse.update.feature,org.eclipse.jgit.ssh.apache,5.5.0.201909110433-r
No repository found containing: osgi.bundle,org.slf4j.api,1.7.2.v20121108-1250
No repository found containing: osgi.bundle,org.slf4j.impl.log4j12,1.7.2.v20131105-2200
Has anyone encountered this issue before or found a way to successfully install EGit on these CubeIDE versions? Any suggestions or workarounds would be greatly appreciated.
Thanks in advance!
iTTy
2026-05-11 1:53 AM
For me it has worked until version 2.0. Now the problem (on an update attempt) is, that the Eclipse Marketplace send a wrong answer. So it really seems to be a marketplace problem. But the Eclipse Foundation has a very inobvious structure and I have no idea where should I file this bug. ST is obviously also thinkung that it is not their problem. As far as an old version of the Egit works for me I could wait for a while, maybe the next update of the Eclipse or the Egit will solve the problem.
Regards,
Dmitry
2026-05-18 8:52 AM
Hello
I think it can be incompatibility problem between stm32cubeide version and Egit version. I am using stm32cube 1.18.1, in market place the latest version of egit is only available for installation. The solution was to dowload the zip file of Egit version 7.0.0 and add install it using install new software section in help
This the link of version 7.0.0: https://www.eclipse.org/downloads/download.php?file=/egit/updates-7.0/org.eclipse.egit.repository-7.0.0.202409031743-r.zip
2026-05-26 12:18 AM
Dear stmobject,
Thankyou for providing the direct download link. I have successfully downlaoded and added EGit to my CubeIDE
Thankyou.
2026-05-26 2:04 AM
Hi @stmobject
May I ask why you choose the release 7.0 and not the latest 7.6 (or 7.7) ?
Was it for compatibility issues ?
In any case, many thanks for the workaround !
If someone form ST could look into this, it would be really helpful !
Cheers
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.