2020-04-19 8:38 AM
We have a STM32MP1 system with no flash media.
How do I push a TF-A/uboot image to DRAM and boot/run from DRAM with
no MMC/flash media ?
2020-04-19 2:27 PM
Figured this out ... simple two line tsv file:
#Opt Id Name Type IP Offset Binary
- 0x01 fsbl1-boot Binary none 0x0 tf-a-stm32mp157c-ya157c-4e512d-trusted.stm32
- 0x03 ssbl-boot Binary none 0x0 u-boot-stm32mp157c-ya157c-4e512d-trusted.stm32
But now how do I also push kernel image and dtb over USB so uboot can boot the kernel.
I tried this but programmer gave a syntax error:
#Opt Id Name Type IP Offset Binary
- 0x01 fsbl1-boot Binary none 0x0 tf-a-stm32mp157c-ya157c-4e512d-trusted.stm32
- 0x03 ssbl-boot Binary none 0x0 u-boot-stm32mp157c-ya157c-4e512d-trusted.stm32
- 0x03 kernel Binary none 0xC2000000 uImage
- 0x03 dtb Binary none 0xC4000000 stm32mp157c.dtb
2020-04-20 12:51 AM
Hi,
I fear it is not possible to start Linux directly using CubeProgrammer, which is intended to program Flash.
Once you have taken the uBoot prompt, maybe look and https://wiki.st.com/stm32mpu/wiki/How_to_boot_the_kernel_via_TFTP_from_U-Boot
and https://wiki.st.com/stm32mpu/wiki/USB_overview#How_to_configure_USB_Gadget_through_configfs which might be used to have an Ethernet over USB if needed.
2020-04-30 12:25 AM
Not possible today but it is planned and coming soon: add a ram0 target.
A other solution it is change the bootcmd to execute a the U-Boot dfu command with ram target when the board is booting from usb and only use STM32CubeProgrammer to load U-boot in DDR, then using dfu-utils to load kernel in DDR.
something like
1/ define dfu ram target with U-Boot variable:
dfu_alt_info=uImage ram ${kernel_addr} 0x2000000;devicetree.dtb ram $[fdt_addr_r} 0x1000000;
2/ update U-boot command
#define STM32MP_BOOTCMD "bootcmd_stm32mp=" \
"echo \"Boot over ${boot_device}${boot_instance}!\";" \
"if test ${boot_device} = serial || test ${boot_device} = usb;" \
- "then stm32prog ${boot_device} ${boot_instance}; " \
+ "then dfu 0 ram 0; bootm ${kernel_addr} ${devicetree_addr};" \
"else " \
"run env_check;" \
"if test ${boot_device} = mmc;" \
"then env set boot_targets \"mmc${boot_instance}\"; fi;" \
"if test ${boot_device} = nand ||" \
" test ${boot_device} = spi-nand ;" \
"then env set boot_targets ubifs0; fi;" \
"run distro_bootcmd;" \
"fi;\0"
not tested, perhaps need some tuning.
regards
2020-07-04 5:50 AM
Hi,
with OpenSTLinux V2.0.0, it is now possible to load and execute a Linux kernel in RAM with STM32CubeProgrammer
#Opt Id Name Type IP Offset Binary
- 0x01 fsbl Binary none 0x0 tf-a.stm32
- 0x03 ssbl Binary none 0x0 u-boot.stm32
P 0x10 kernel System ram0 0xC2000000 uImage.bin
P 0x11 dtb FileSytem ram0 0xC4000000 stm32mp157c.dtb
Regards
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.