2026-05-01 1:10 AM
Hi ST Dev team!
I have found that LSE is mandatory when building a new custom board. If not LSE is mounted and configured, then both TF-A and Op-tee will complaining about clock ID 5, which is LSE.
Here is a walk around for Op-tee by removing the &clk-lse.
And for TF-A, ut must need some modification inside the code:
Processor: STM32MP257F
2026-05-05 4:48 AM
Hello @DMårt
Thank you for pointing that out. It should also be fixed in OpenSTLinux DV6.2.
https://wiki.st.com/stm32mpu/wiki/STM32_MPU_OpenSTLinux_release_note_-_v6.2.0
Best Regards,
Olivier
2026-05-09 1:26 AM
No, it has not!
I build the official manifest from ST
repo init -u https://github.com/STMicroelectronics/oe-manifest.git -b refs/tags/openstlinux-6.6-yocto-scarthgap-mpu-v26.02.18
And it gave me this:
This time, the output says clk-lse, instead of CLK ID = 5.
NOTICE: Early console setup
NOTICE: CPU: STM32MP257FAK Rev.Y
NOTICE: Model: STMicroelectronics STM32MP257F-DK STM32CubeMX board - openstlinux-6.6-yocto-scarthgap-mpu-v26.02.18
NOTICE: Reset reason: Power-on reset (por_rstn) (0x2035)
INFO: PMIC2 version = 0x11
INFO: PMIC2 product ID = 0x21
INFO: FCONF: Reading TB_FW firmware configuration file from: 0xe011000
INFO: FCONF: Reading firmware configuration information for: stm32mp_io
INFO: FCONF: Reading firmware configuration information for: stm32mp_fuse
INFO: Using SDMMC
INFO: Instance 1
INFO: Boot used partition fsbl1
NOTICE: BL2: v2.10-stm32mp2-r2.0(debug):lts-v2.10.24-dirty(a07367a1)
NOTICE: BL2: Built : 16:16:36, Oct 3 2025
INFO: BL2: Loading image id 26
INFO: Loading image id=26 at address 0xe041000
INFO: Image id=26 loaded: 0xe041000 - 0xe049650
INFO: BL2: Doing platform setup
INFO: RAM: LPDDR4 32bits 1200000kHz
INFO: Memory size = 0x80000000 (2048 MB)
INFO: BL2: Loading image id 1
INFO: Loading image id=1 at address 0xe000000
INFO: Image id=1 loaded: 0xe000000 - 0xe000326
INFO: FCONF: Reading FW_CONFIG firmware configuration file from: 0xe000000
INFO: FCONF: Reading firmware configuration information for: dyn_cfg
INFO: FCONF: Reading firmware configuration information for: risaf_config
INFO: RISAF2: No configuration in DT, use default
INFO: BL31 max size = 0x17000 (94208B)
INFO: BL2: Loading image id 3
INFO: Loading image id=3 at address 0xe000000
INFO: Image id=3 loaded: 0xe000000 - 0xe0169f0
INFO: BL2: Loading image id 19
INFO: Loading image id=19 at address 0x81fc0000
INFO: Image id=19 loaded: 0x81fc0000 - 0x81fc3b2c
INFO: BL2: Loading image id 4
INFO: Loading image id=4 at address 0x82000000
INFO: Image id=4 loaded: 0x82000000 - 0x8200001c
INFO: OPTEE ep=0x82000000
INFO: OPTEE header info:
INFO: magic=0x4554504f
INFO: version=0x2
INFO: arch=0x1
INFO: flags=0x0
INFO: nb_images=0x1
INFO: BL2: Loading image id 8
INFO: Loading image id=8 at address 0x82000000
INFO: Image id=8 loaded: 0x82000000 - 0x821087b8
INFO: BL2: Loading image id 2
INFO: Loading image id=2 at address 0x84400000
INFO: Image id=2 loaded: 0x84400000 - 0x8441c768
INFO: BL2: Loading image id 5
INFO: Loading image id=5 at address 0x84000000
INFO: Image id=5 loaded: 0x84000000 - 0x841d54b8
NOTICE: BL2: Booting BL31
INFO: Entry point address = 0xe000000
INFO: SPSR = 0x3cd
NOTICE: Early console setup
INFO: ARM GICv2 driver initialized
NOTICE: BL31: v2.10-stm32mp2-r2.0(debug):lts-v2.10.24-dirty(a07367a1)
NOTICE: BL31: Built : 16:16:36, Oct 3 2025
INFO: BL31: Initializing runtime services
INFO: BL31: Initializing BL32
I/TC: Early console on UART#6
D/TC:0 add_phys_mem:674 VCORE_UNPG_RX_PA type TEE_RAM_RX 0x82000000 size 0x000fd000
D/TC:0 add_phys_mem:674 VCORE_UNPG_RW_PA type TEE_RAM_RW 0x820fd000 size 0x00303000
D/TC:0 add_phys_mem:674 ta_base type TA_RAM 0x82400000 size 0x01c00000
D/TC:0 add_phys_mem:674 SRAM1_BASE type RAM_SEC 0x0e040000 size 0x00001000
D/TC:0 add_phys_mem:674 DBGMCU_BASE type IO_NSEC 0x4a000000 size 0x00200000
D/TC:0 add_phys_mem:674 GIC_BASE type IO_SEC 0x4ac00000 size 0x00200000
D/TC:0 add_phys_mem:674 SAHB_BASE type IO_SEC 0x46200000 size 0x01e00000
D/TC:0 add_phys_mem:674 SAPB_BASE type IO_SEC 0x46000000 size 0x00200000
D/TC:0 add_phys_mem:674 AHB5_BASE type IO_SEC 0x48200000 size 0x01e00000
D/TC:0 add_phys_mem:674 AHB4_BASE type IO_SEC 0x44200000 size 0x01e00000
D/TC:0 add_phys_mem:674 AHB3_BASE type IO_SEC 0x42000000 size 0x02000000
D/TC:0 add_phys_mem:674 AHB2_BASE type IO_SEC 0x40400000 size 0x01c00000
D/TC:0 add_phys_mem:674 APB4_BASE type IO_SEC 0x48000000 size 0x00200000
D/TC:0 add_phys_mem:674 APB3_BASE type IO_SEC 0x44000000 size 0x00200000
D/TC:0 add_phys_mem:674 APB2_BASE type IO_SEC 0x40200000 size 0x00200000
D/TC:0 add_phys_mem:674 APB1_BASE type IO_SEC 0x40000000 size 0x00200000
D/TC:0 add_phys_mem:674 APB1_BASE type IO_NSEC 0x40000000 size 0x00200000
D/TC:0 add_va_space:714 type RES_VASPACE size 0x02000000
D/TC:0 add_va_space:714 type SHM_VASPACE size 0x02000000
D/TC:0 dump_mmap_table:844 type TA_RAM va 0x70c00000..0x727fffff pa 0x82400000..0x83ffffff size 0x01c00000 (pgdir)
D/TC:0 dump_mmap_table:844 type IO_SEC va 0x72a00000..0x72bfffff pa 0x4ac00000..0x4adfffff size 0x00200000 (pgdir)
D/TC:0 dump_mmap_table:844 type IO_NSEC va 0x72c00000..0x72dfffff pa 0x4a000000..0x4a1fffff size 0x00200000 (pgdir)
D/TC:0 dump_mmap_table:844 type IO_SEC va 0x72e00000..0x74bfffff pa 0x48200000..0x49ffffff size 0x01e00000 (pgdir)
D/TC:0 dump_mmap_table:844 type IO_SEC va 0x74e00000..0x74ffffff pa 0x48000000..0x481fffff size 0x00200000 (pgdir)
D/TC:0 dump_mmap_table:844 type IO_SEC va 0x75000000..0x76dfffff pa 0x46200000..0x47ffffff size 0x01e00000 (pgdir)
D/TC:0 dump_mmap_table:844 type IO_SEC va 0x77000000..0x771fffff pa 0x46000000..0x461fffff size 0x00200000 (pgdir)
D/TC:0 dump_mmap_table:844 type IO_SEC va 0x77200000..0x78ffffff pa 0x44200000..0x45ffffff size 0x01e00000 (pgdir)
D/TC:0 dump_mmap_table:844 type IO_SEC va 0x79200000..0x793fffff pa 0x44000000..0x441fffff size 0x00200000 (pgdir)
D/TC:0 dump_mmap_table:844 type IO_SEC va 0x79400000..0x7b3fffff pa 0x42000000..0x43ffffff size 0x02000000 (pgdir)
D/TC:0 dump_mmap_table:844 type IO_SEC va 0x7b600000..0x7d1fffff pa 0x40400000..0x41ffffff size 0x01c00000 (pgdir)
D/TC:0 dump_mmap_table:844 type IO_SEC va 0x7d400000..0x7d5fffff pa 0x40200000..0x403fffff size 0x00200000 (pgdir)
D/TC:0 dump_mmap_table:844 type IO_NSEC va 0x7d600000..0x7d7fffff pa 0x40000000..0x401fffff size 0x00200000 (pgdir)
D/TC:0 dump_mmap_table:844 type IO_SEC va 0x7d800000..0x7d9fffff pa 0x40000000..0x401fffff size 0x00200000 (pgdir)
D/TC:0 dump_mmap_table:844 type RES_VASPACE va 0x7da00000..0x7f9fffff pa 0x00000000..0x01ffffff size 0x02000000 (pgdir)
D/TC:0 dump_mmap_table:844 type SHM_VASPACE va 0x7fc00000..0x81bfffff pa 0x00000000..0x01ffffff size 0x02000000 (pgdir)
D/TC:0 dump_mmap_table:844 type RAM_SEC va 0x81fff000..0x81ffffff pa 0x0e040000..0x0e040fff size 0x00001000 (smallpg)
D/TC:0 dump_mmap_table:844 type TEE_RAM_RX va 0x82000000..0x820fcfff pa 0x82000000..0x820fcfff size 0x000fd000 (smallpg)
D/TC:0 dump_mmap_table:844 type TEE_RAM_RW va 0x820fd000..0x823fffff pa 0x820fd000..0x823fffff size 0x00303000 (smallpg)
D/TC:0 core_mmu_xlat_table_alloc:526 xlat tables used 1 / 5
D/TC:0 core_mmu_xlat_table_alloc:526 xlat tables used 2 / 5
D/TC:0 core_mmu_xlat_table_alloc:526 xlat tables used 3 / 5
D/TC:0 core_mmu_xlat_table_alloc:526 xlat tables used 4 / 5
I/TC:
I/TC: Embedded DTB found
D/TC:0 0 core_mmu_set_discovered_nsec_ddr:494 Non-secure memory range [0x80000000 0x82000000]
D/TC:0 0 core_mmu_set_discovered_nsec_ddr:494 Non-secure memory range [0x84000000 0x100000000]
I/TC: OP-TEE version: 4.0.0-dev (gcc version 13.4.0 (GCC)) #1 Fri Oct 20 18:29:31 UTC 2023 aarch64
I/TC: WARNING: This OP-TEE configuration might be insecure!
I/TC: WARNING: Please check https://optee.readthedocs.io/en/latest/architecture/porting_guidelines.html
I/TC: Primary CPU initializing
D/TC:0 0 call_preinitcalls:21 level 2 mobj_mapped_shm_init()
D/TC:0 0 mobj_mapped_shm_init:470 Shared memory address range: 7fc00000, 81c00000
D/TC:0 0 call_initcalls:40 level 1 initialize_bsec()
D/TC:0 0 initialize_nvmem_layout_from_dt:1416 nvmem[1] = part_number_otp 9bit offset: 0, length: 32
D/TC:0 0 initialize_nvmem_layout_from_dt:1416 nvmem[2] = package_otp 122bit offset: 0, length: 0
D/TC:0 0 initialize_nvmem_layout_from_dt:1416 nvmem[3] = otp124 124bit offset: 0, length: 32
D/TC:0 0 initialize_nvmem_layout_from_dt:1416 nvmem[4] = otp144 144bit offset: 0, length: 256
D/TC:0 0 initialize_nvmem_layout_from_dt:1416 nvmem[5] = oem_rproc_pkh 176bit offset: 0, length: 256
D/TC:0 0 initialize_nvmem_layout_from_dt:1416 nvmem[6] = otp260 260bit offset: 0, length: 256
D/TC:0 0 initialize_nvmem_layout_from_dt:1416 nvmem[7] = oem_rproc_enc_key 336bit offset: 0, length: 256
D/TC:0 0 initialize_nvmem_layout_from_dt:1416 nvmem[8] = otp352 352bit offset: 0, length: 256
D/TC:0 0 initialize_nvmem_layout_from_dt:1416 nvmem[9] = otp360 360bit offset: 0, length: 128
D/TC:0 0 initialize_nvmem_layout_from_dt:1416 nvmem[10] = otp364 364bit offset: 0, length: 128
D/TC:0 0 call_initcalls:40 level 1 clk_dt_probe()
D/TC:0 0 clk_dt_probe:207 Probing clocks from devicetree
F/TC:0 0 probe_driver_node:543 Probing fixed_clock on node clk-hse
D/TC:0 0 clk_register:136 Registered clock clk-hse, freq 24000000
D/TC:0 0 probe_driver_node:550 element: fixed_clock on node clk-hse initialized
F/TC:0 0 probe_driver_node:543 Probing fixed_clock on node clk-hsi
D/TC:0 0 clk_register:136 Registered clock clk-hsi, freq 64000000
D/TC:0 0 probe_driver_node:550 element: fixed_clock on node clk-hsi initialized
F/TC:0 0 probe_driver_node:543 Probing fixed_clock on node clk-lsi
D/TC:0 0 clk_register:136 Registered clock clk-lsi, freq 32000
D/TC:0 0 probe_driver_node:550 element: fixed_clock on node clk-lsi initialized
F/TC:0 0 probe_driver_node:543 Probing fixed_clock on node clk-msi
D/TC:0 0 clk_register:136 Registered clock clk-msi, freq 16000000
D/TC:0 0 probe_driver_node:550 element: fixed_clock on node clk-msi initialized
F/TC:0 0 probe_driver_node:543 Probing fixed_clock on node clk-i2sin
D/TC:0 0 clk_register:136 Registered clock clk-i2sin, freq 0
D/TC:0 0 probe_driver_node:550 element: fixed_clock on node clk-i2sin initialized
F/TC:0 0 probe_driver_node:543 Probing fixed_clock on node clk-rcbsec
D/TC:0 0 clk_register:136 Registered clock clk-rcbsec, freq 64000000
D/TC:0 0 probe_driver_node:550 element: fixed_clock on node clk-rcbsec initialized
E/TC:0 0 parse_clock_property:82 Probe parent clock node clk-lse on node rcc@44200000: 0xffff0008
E/TC:0 0 Panic at /usr/src/debug/optee-os-stm32mp/4.0.0-stm32mp-r3/core/drivers/clk/clk_dt.c:85 <parse_clock_property>
E/TC:0 0 TEE load address @ 0x82000000
E/TC:0 0 Call stack:
E/TC:0 0 0x82008180
E/TC:0 0 0x820473cc
E/TC:0 0 0x8203634c
E/TC:0 0 0x820363dc
E/TC:0 0 0x82036418
E/TC:0 0 0x82036418
E/TC:0 0 0x820366b4
E/TC:0 0 0x820490d4
E/TC:0 0 0x82007bec
E/TC:0 0 0x82007f84
2026-05-09 2:06 AM - edited 2026-05-09 10:33 AM
Hi! @OlivierK
Add this patch to your meta-st layer in https://github.com/STMicroelectronics/meta-st-stm32mp/tree/scarthgap/recipes-bsp/trusted-firmware-a/tf-a-stm32mp
Patch: See attached file
From aef2af78f34f6d9ae91dae9191d8a07b0d419f95 Mon Sep 17 00:00:00 2001
From: noname <noreply@example.com>
Date: Sat, 9 May 2026 10:40:59 +0200
Subject: [PATCH 2/2] Avoid LSE temporary
---
drivers/st/clk/clk-stm32-core.c | 4 ++++
1 file changed, 4 insertions(+)
diff --git a/drivers/st/clk/clk-stm32-core.c b/drivers/st/clk/clk-stm32-core.c
index 8c2f5a96a..709676217 100644
--- a/drivers/st/clk/clk-stm32-core.c
+++ b/drivers/st/clk/clk-stm32-core.c
@@ -453,6 +453,10 @@ int clk_stm32_enable_call_ops(struct stm32_clk_priv *priv, uint16_t id)
}
if ((ops->is_enabled != NULL) && !ops->is_enabled(priv, id)) {
+ if (id == 5) {
+ WARN("PATCH: clk_stm32_enable_call_ops: ignoring clk id 5 (clk-lse) failure\n");
+ return 0;
+ }
ERROR("failed to enable clock id: %u\n", id);
panic();
}
--
2.43.0After that you need to rename clock-names and clocks to exclude &clk-lse in optee DT.
&rcc {
status = "okay";
/* USER CODE BEGIN rcc */
/* Excluding <&clk-lse> */
clocks = <&clk_hse>, <&clk_hsi>, <&clk_lsi>, <&clk_msi>, <&clk_i2sin>;
clock-names = "clk-hse", "clk-hsi", "clk-lsi", "clk-msi", "clk-i2sin";
st,c1msrd = <2>;
st,clk_opp{
st,ck_cpu1{
cfg_1{
hz = <1500000000>;
st,pll = <&pll1_cfg_1500MHz>;
};
cfg_2{
hz = <1200000000>;
st,pll = <&pll1_cfg_1200MHz>;
};
};
st,ck_gpu{
cfg_1{
hz = <800000000>;
st,pll = <&pll3_cfg_800MHz>;
};
cfg_2{
hz = <900000000>;
st,pll = <&pll3_cfg_900MHz>;
};
};
};
/* USER CODE END rcc */
};
2026-05-14 1:08 PM
More information that LSE-bug is not fixed yet.
mint@mint-ThinkPad-W540:~/Documents/Github/Watermelon-Wine-1A/watermelon-wine-os/layers/meta-st/meta-st-stm32mp-addons$ git log --oneline -n 10
3597fb3 (HEAD, tag: openstlinux-6.6-yocto-scarthgap-mpu-v26.02.18, m/refs/tags/openstlinux-6.6-yocto-scarthgap-mpu-v26.02.18, OpenSTLinux/scarthgap) CUBEMX-STM32MP: configure use of CUBEMX_M33_TZ
c67adfc MACHINE: set m33fw default configuration
9322326 M33TDPROJECTS-STARTER-STM32MP2: set specific CubeMX configuration
9298ce1 MACHINE: enable external tf-m platform profile from CubeMX project
ca6f576 MACHINE: update for CubeMX tf-m platform source
8078626 MACHINE: update for m33fw configuration
9eb0628 M33TDPROJECTS-STARTER-STM32MP2: update folder name
6d5e442 MACHINE: force use of CUBEMX_DTB on extlinux.conf file
d6f276a M4PROJECTS-STM32MP1: update folder name
15be8c7 M33TDPROJECTS-STARTER-STM32MP2: fix missing inherit for CubeMX class
mint@mint-ThinkPad-W540:~/Documents/Github/Watermelon-Wine-1A/watermelon-wine-os/layers/meta-st/meta-st-stm32mp-addons$ cd ..
mint@mint-ThinkPad-W540:~/Documents/Github/Watermelon-Wine-1A/watermelon-wine-os/layers/meta-st$ cd meta-st-stm32mp
mint@mint-ThinkPad-W540:~/Documents/Github/Watermelon-Wine-1A/watermelon-wine-os/layers/meta-st/meta-st-stm32mp$ git log --oneline -n 10
e53460d (HEAD, tag: openstlinux-6.6-yocto-scarthgap-mpu-v26.02.18, m/refs/tags/openstlinux-6.6-yocto-scarthgap-mpu-v26.02.18) Update SBOM on EULA
6caba0f SDK-INFOS: fix typo and align examples
5007f7f CUBE MP2: 1.3.0
df3a656 EXTERNAL-DT: v6.0-stm32mp-r3
db192f8 KERNEL: v6.6-stm32mp-r3
ec7b429 TF-A: v2.10-stm32mp-r3
fb55b14 TF-M: v2.1.3-stm32mp-r2
2d48668 TF-M: v2.1.3-stm32mp-r2
1bfbbd0 U-BOOT: v2023.10-stm32mp-r3
cda5991 OPTEE: 4.0.0-stm32mp-r3
mint@mint-ThinkPad-W540:~/Documents/Github/Watermelon-Wine-1A/watermelon-wine-os/layers/meta-st/meta-st-stm32mp$ cd ..
mint@mint-ThinkPad-W540:~/Documents/Github/Watermelon-Wine-1A/watermelon-wine-os/layers/meta-st$ cd meta-st-openstlinux/
mint@mint-ThinkPad-W540:~/Documents/Github/Watermelon-Wine-1A/watermelon-wine-os/layers/meta-st/meta-st-openstlinux$ git log --oneline -n 10
993e43a (HEAD, tag: openstlinux-6.6-yocto-scarthgap-mpu-v26.02.18, m/refs/tags/openstlinux-6.6-yocto-scarthgap-mpu-v26.02.18, OpenSTLinux/scarthgap) OPTEE ADDONS: License, code of conduct
e21bbfb LICENSE management: manage splitted partitions
b58df11 DCMIPP ISP: histogram
4d95d93 EVENT GTK, WESTON CUBE: add code of conduct
cbe39f5 libcamera: 0.3.0 with ST IPA
66b4af2 PKGGROUP: add libcamera
2a3dd12 INITRD: load kernel module before resize
425bdc4 IMAGE: add M33TD splashscreen and service
c7ad3bd INITRD: use kmod instead of busybox kmod
d5228dc PKG OPTEE: cleanup
mint@mint-ThinkPad-W540:~/Documents/Github/Watermelon-Wine-1A/watermelon-wine-os/layers/meta-st/meta-st-openstlinux$
``
2026-05-24 4:12 AM
Hi @OlivierK
Any news about this?
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.