2020-10-23 6:33 AM
Hi,
I'm having an issue while trying to debug the OpenAMP_TTY_ECHO_CM4 example described in gettin' started guide for stm32mp157a-DK1 (here link) using Cude IDE 1.4.2 on windows 10 machine. I configure the debug session as describe in the guide section 7, but when I started it, I got the following messages:
Open On-Chip Debugger 0.10.0+dev-g30d1303 (2020-06-18-09:13)
Licensed under GNU GPL v2
For bug reports, read
http://openocd.org/doc/doxygen/bugs.html
srst_only srst_pulls_trst srst_gates_jtag srst_open_drain connect_deassert_srst
Info : Listening on port 6666 for tcl connections
Info : Listening on port 4444 for telnet connections
Info : STLINK V2J37M26 (API v2) VID:PID 0483:3752
Info : Target voltage: 3.220093
Info : Unable to match requested speed 8000 kHz, using 4000 kHz
Info : Unable to match requested speed 8000 kHz, using 4000 kHz
Info : clock speed 4000 kHz
Info : stlink_dap_op_connect(connect)
Info : SWD DPIDR 0x6ba02477
Info : stlink_dap_op_connect(connect)
Info : SWD DPIDR 0x6ba02477
Info : STM32MP157CAAx.cm4: hardware has 6 breakpoints, 4 watchpoints
Info : STM32MP157CAAx.cpu0: hardware has 6 breakpoints, 4 watchpoints
Info : STM32MP157CAAx.cpu1: hardware has 6 breakpoints, 4 watchpoints
Info : STM32MP157CAAx.cm4: external reset detected
Info : starting gdb server for STM32MP157CAAx.cpu0 on 3334
Info : Listening on port 3334 for gdb connections
Info : starting gdb server for STM32MP157CAAx.cm4 on 3333
Info : Listening on port 3333 for gdb connections
Info : accepting 'gdb' connection on tcp/3333
Info : Halt timed out, wake up GDB.
Error: timed out while waiting for target halted
Error executing event gdb-attach on target STM32MP157CAAx.cm4:
Info : New GDB Connection: 1, Target STM32MP157CAAx.cm4, state: reset
Warn : negative reply, retrying
Warn : negative reply, retrying
Warn : target not halted
Info : target STM32MP157CAAx.cm4 was not halted when resume was requested
When I reopen a serial console on cube IDE to run the test (according to guide section 8), I can't find any /dev/ttyRPMSG0 or /dev/ttyRPMSG1 device.
Please someone could help?
Marco.
Solved! Go to Solution.
2020-10-29 2:47 AM
Hi @MBassi ,
Straight forward solution is to download again the starter package from st.com and reflash it on board.
Second solution is to update dropbear version on target using apt-get service as per advice here :
https://wiki.st.com/stm32mpu/wiki/STM32MP15_OpenSTLinux_release_note#Main_restrictions_list
Third solution is application of the patch and generation of a new image using Distribution package.
https://wiki.st.com/stm32mpu/wiki/STM32MP1_Distribution_Package
Hope it help,
Olivier
2020-10-23 6:47 AM
Thank you for the question Marco, I have your same problem when trying to start the debug session with CubeIDE.
I've successfully tried manual start of the demo application via "remoteproc" and also the debug in Reserved (Engineering) mode. But the Production Mode debug on the M4 won't start.
I hope someone could help us!
2020-10-27 1:40 AM
Hi all, i still have the same problem, even with a fresh install of both the environment and IDE.
Anyone else is experiencing this problem or would help?
2020-10-27 8:03 AM
Hi,
I also tryed using the cube IDE 1.4.2 for Ubuntu OS but I got the same debugging issue.
Hope someone could help
2020-10-27 9:07 AM
I have this issue too, I think it might be because the example is for the dk2 devboard which has a slightly different cpu but it's not clear
2020-10-27 9:35 AM
In the debugger options, under configuration script you can show the options and change connection speed to 4mhz.. this gets rid of that error but still has a target halted issue
2020-10-28 7:57 AM
Hi @MBassi , @Raggio ,
This issue really looks like the known "STM32CubeIDE vs OpenSTLinux misalignement on “ciphers�? as highlighted in the "pin" post :
Symptom : Prevent to load M4 firmware in Production mode
Seen in post : https://community.st.com/s/question/0D53W00000G1PG8SAN/update-stm32cubeide-version-142-stopped-sending-firmware-to-mpu
Starter package : fixed
Developper Package : not visible
Distribution package : Patch delivered on github
Can you pleas check ?
Thx
Olivier
2020-10-28 10:05 AM
Hi @Community member
Thanks for answer me, I read the posts you linked in your reply. I use a customized version of dunfell release, so I have to use the github link to download (I used git command) a patch file, but the file I get doesn't seem I patch file. I'm new in kernel recompiling so maybe I miss something about patching procedure,
please could you help me
Marco.
2020-10-29 1:46 AM
I managed to connect /run the program with breakpoints using a much lower connection speed in the khz range, started at the lowest and looking to see how high it can get as it's a bit slow to use at the lowest settings
2020-10-29 2:27 AM
Thanks @OHaza.1
I tryed to lower connection down to khz speed but my issue remains.
I thinks the solution posted by Olivier could suit better my case, but I have to understand how to apply the changes on my dunfell costumized release.
At the moment I don't known where/how to apply the changes present in the github link: I can't use the repository directly because it's part of bitbake layers system but I use a differt compile chain
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.