STM32 MPUs Software development tools

Ask questions and find answers on STM32 microprocessors software development tools.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32CubeIDE 2.1.1 released

We are pleased to announce that the minor version 2.1.1 of STM32CubeIDE is available. What is new in 2.1.1: This release covers the topics listed below: SEGGER J-Link GDB server updated to 9.24 to fix an issue with the Live Expression view during the...

Aimen1 by ST Employee
  • 505 Views
  • 0 replies
  • 0 kudos

STM32CubeMX 6.17.0 released

We are pleased to announce that version 6.17.0 of STM32CubeMX is available. What is new in 6.17.0: Added support for new microcontrollers across the STM32WBA, STM32H5, and STM32U3 seriesAdded support for new boards: NUCLEO-WBA25CE1, NUCLEO-H5E5ZJ, ST...

Aimen1 by ST Employee
  • 392 Views
  • 0 replies
  • 0 kudos

STM32CubeProgrammer v2.22 released

We are pleased to announce that STM32CubeProgrammer 2.22 is available What is new in 2.22: Support for the STM32U3 microcontrollers with 2 Mbytes of flash memory: Internal memory programming through debug and bootloader interfacesOption bytes program...

Resolved! secure boot and stm32key from

Hi, All. In the wiki, the process to program the PKH into the OTP is done with stm32key tool in u-boot. Also, PKH file must be available in a filesystem partition. All these tasks need to be done manually...Is it possible to do this same process from...

AVazquez by Associate III
  • 1724 Views
  • 2 replies
  • 0 kudos

Resolved! Pin MODE for peripherals not set correctly in device tree output file produced by CubeMx

Pin MODE for peripherals are set incorrectly with RSVD instead of correct alternate function definition (AF13).When building uboot it failed because pin Mode "RSVD" is incorrectly defined.e.g code from device tree   m4_dcmi_pins_mx: m4_dcmi_mx-0 {   ...

Resolved! ERROR: Partition ssbl not found from TF-A

I am trying to boot U-boot as SSBL on a simple board with an eMMC flash.I flash the partitions using the embedded DFU ROMboot with STM32CubeProgrammer using the following Flash Layout#Opt   Id Name   Type   IP Offset Binary-  0x01   fsbl1-boot Binary...

CErik.1 by Associate II
  • 5001 Views
  • 4 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.