2020-09-18 1:54 AM
Pin MODE for peripherals are set incorrectly with RSVD instead of correct alternate function definition (AF13).
When building uboot it failed because pin Mode "RSVD" is incorrectly defined.
e.g code from device tree
m4_dcmi_pins_mx: m4_dcmi_mx-0 {
pins {
pinmux = <STM32_PINMUX('A', 6, RSVD)>, /* DCMI_PIXCLK */
<STM32_PINMUX('E', 0, RSVD)>, /* DCMI_D2 */
<STM32_PINMUX('E', 1, RSVD)>, /* DCMI_D3 */
<STM32_PINMUX('F', 11, RSVD)>, /* DCMI_D12 */
<STM32_PINMUX('H', 8, RSVD)>, /* DCMI_HSYNC */
<STM32_PINMUX('H', 9, RSVD)>, /* DCMI_D0 */
<STM32_PINMUX('H', 10, RSVD)>, /* DCMI_D1 */
<STM32_PINMUX('H', 14, RSVD)>, /* DCMI_D4 */
<STM32_PINMUX('H', 15, RSVD)>, /* DCMI_D11 */
<STM32_PINMUX('I', 0, RSVD)>, /* DCMI_D13 */
<STM32_PINMUX('I', 1, RSVD)>, /* DCMI_D8 */
<STM32_PINMUX('I', 2, RSVD)>, /* DCMI_D9 */
<STM32_PINMUX('I', 3, RSVD)>, /* DCMI_D10 */
<STM32_PINMUX('I', 4, RSVD)>, /* DCMI_D5 */
<STM32_PINMUX('I', 5, RSVD)>, /* DCMI_VSYNC */
<STM32_PINMUX('I', 6, RSVD)>, /* DCMI_D6 */
<STM32_PINMUX('I', 7, RSVD)>; /* DCMI_D7 */
};
};
m4_i2c2_pins_mx: m4_i2c2_mx-0 {
pins {
pinmux = <STM32_PINMUX('H', 4, RSVD)>, /* I2C2_SCL */
<STM32_PINMUX('H', 5, RSVD)>; /* I2C2_SDA */
};
};
When checked in CubeMx configuration is correctly set (including GPIO mode), and also in the "pinout view" pins are set with correct Alternate function.
I am using CubeMX version 6.0.1, and working on SM32MP157cac project.
Question is why CubeMx is outputing RSVD instead of AF13 for pin mode?
Solved! Go to Solution.
2020-09-25 6:47 AM
Hi @BalaGajenthan ,
Well, RSVD stands for "Reserved". This allows to signal to the Resource Manager (which makes the link between the world A7 and M4) that the IO is used and especially assigned to M4 (Using A7 for expl, you will get AFx instead of RSVD).
With this info the Resources Manager will be able to manage any conflict with the EXTI depending on whether or not they are used by the M4.
Best Regards,
Khouloud
2020-09-25 2:12 AM
Hello @BalaGajenthan
Thanks for the feedback, it will be internally checked then I'll come back to you.
Best Regards,
Khouloud
2020-09-25 6:47 AM
Hi @BalaGajenthan ,
Well, RSVD stands for "Reserved". This allows to signal to the Resource Manager (which makes the link between the world A7 and M4) that the IO is used and especially assigned to M4 (Using A7 for expl, you will get AFx instead of RSVD).
With this info the Resources Manager will be able to manage any conflict with the EXTI depending on whether or not they are used by the M4.
Best Regards,
Khouloud
2020-09-25 9:09 AM
Hi @Khouloud ZEMMELI
Thanks for you reply.
The peripherals in question are mutally exclusive to M4 or A7.
I tried to assign it to A7 and it does produce the corrcect device tree with AFx. but I want to assign it to M4 only, in this case it should not create a device tree block for it right?
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.