STM32 MPUs Software development tools

Ask questions and find answers on STM32 microprocessors software development tools.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32CubeIDE 2.1.1 released

We are pleased to announce that the minor version 2.1.1 of STM32CubeIDE is available. What is new in 2.1.1: This release covers the topics listed below: SEGGER J-Link GDB server updated to 9.24 to fix an issue with the Live Expression view during the...

Aimen1 by ST Employee
  • 505 Views
  • 0 replies
  • 0 kudos

STM32CubeMX 6.17.0 released

We are pleased to announce that version 6.17.0 of STM32CubeMX is available. What is new in 6.17.0: Added support for new microcontrollers across the STM32WBA, STM32H5, and STM32U3 seriesAdded support for new boards: NUCLEO-WBA25CE1, NUCLEO-H5E5ZJ, ST...

Aimen1 by ST Employee
  • 392 Views
  • 0 replies
  • 0 kudos

STM32CubeProgrammer v2.22 released

We are pleased to announce that STM32CubeProgrammer 2.22 is available What is new in 2.22: Support for the STM32U3 microcontrollers with 2 Mbytes of flash memory: Internal memory programming through debug and bootloader interfacesOption bytes program...

Resolved! EXTI lineX is automatically disabled.

1. Select STM32MP151A2. Select an GPIOx and set to GIPIO_EXTx3.Select again GPIO under Pinout View, right click -> Pin Reserved -> Cortex-M44. Goto NVIC: EXTI lineX interrupt Enable Check.5. Select any of the peripheral devices, enable Cortex-A7 or C...

HAPPYDAY by Associate II
  • 1750 Views
  • 2 replies
  • 0 kudos

Resolved! EMMC Questions

Hi ST Teams!We've made a custom board with sdcard and mmc, all these device can be viewed from uboot/linux userspace. We are mainly using starter kit (v1.2) with modified tfa/uboot.For mmc programming, using Cube Programmer CLI(v2.5) we have only uar...

Eldam by Senior
  • 5006 Views
  • 6 replies
  • 0 kudos

cube programmer sd card image download- STM32MP1

These are log i got during download, any clueSTM32_Programmer_CLI -c port=usb1 -tm 20000 -w flashlayout_mp1som-image/FlashLayout_sdcard_mp1som-mystm32mp1-basic.tsv    -------------------------------------------------------------------                ...

Ara.1 by Senior
  • 3468 Views
  • 7 replies
  • 0 kudos

SSH Connection to STM32CUBEIDE

Hi,How can I connect to STM32MPU via SSH from inside STM32CUBEIDE.?? Is there a way we can do that?This really helps in live debug of things.Alternatively is there a way I can live debug an application running on A7?

NPal.2 by Senior
  • 2521 Views
  • 3 replies
  • 0 kudos

stm32mp1 uart noise rx

Hi All,i am using stm32mp1 cpu,, recently i m facing floating rx issue on debug uart, with physical debug cable , i could default state of RX lines were pull up, and when i remove the cable, the RX lines is floating and its voltage fluctuates between...

Ara.1 by Senior
  • 3884 Views
  • 5 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.