2022-10-06 8:12 AM
We have also deleted the OTG (USBC) hardware and have commented out the code to check for the OTG power., Otherwise we are using the basic defconfig and the DK2 devtree.
2022-10-10 12:54 AM
Hello @nonesuchetter ,
ECMF02-2AMX6 is used to protect from ESD and EMI, it should work without it.
What is the problem that you encounter with the USB port 1? Do you have an error?
The port related to OTG is the port 2:
https://wiki.st.com/stm32mpu/wiki/USBPHYC_device_tree_configuration#DT_bindings_documentation
Can you explain the modifications that you made, because you normally doesn't need to modify code part:
We have also deleted the OTG (USBC) hardware and have commented out the code to check for the OTG power.,May I know which Ecosystem are you using and please can you indicate the file that you are using when you say "using the basic defconfig" ?
To help you, I will also need the traces made during the boot by your board.
Best Regards,
Kevin
2022-10-11 6:09 AM
2022-10-12 6:18 AM
For some reason my answer didn't come through. I include it here.
What is the problem that you encounter with the USB port 1? Do you have an error?
The port doesn't reset.
The port related to OTG is the port 2:
https://wiki.st.com/stm32mpu/wiki/USBPHYC_device_tree_configuration#DT_bindings_documentation
Can you explain the modifications that you made, because you normally doesn't need to modify code part:
Commented out board_check_usb_power();
in board/st/stm32mp1/stm32mp1.c
We have also deleted the OTG (USBC) hardware and have commented out the code to check for the OTG power.,
May I know which Ecosystem are you using and please can you indicate the file that you are using when you say "using the basic defconfig" ?
Ecosystem-v3.1.0 Build u-boot as follows:
make stm32mp15_basic_defconfig
make menuconfig (to enable debug log)
make -DEVICE_TREE=stm32mp157c-dk2 all
To help you, I will also need the traces made during the boot by your board.
I have attached the u-boot startup log as well as the usb start log. Attached to the USB A (dm1, dp1) port is a full speed device, a ZIP 250 drive.
2022-10-12 6:19 AM
2022-10-28 8:43 AM
Hi @nonesuchetter ,
Are you aware that ST does not recommend and support product using basic_defconfig ?
It's remains present on 3.1 ecosystem as a legacy to build the U-Boot SPL flavor require for DDR test and tuning.
In link below it's stated that Uboot-SPL has a very limited feature set
https://wiki.st.com/stm32mpu-ecosystem-v1/wiki/Boot_chains_overview#Boot_chains_features_set
Maybe you are fully aware and already handle this, but anyway, ST cannot support you really further in this direction.
Any rational to not use trusted config?
Olivier
2022-10-28 8:07 PM
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.