2024-02-15 5:10 AM - edited 2024-02-15 5:20 AM
Hi All,
i am using stmp157 customize board, with linux yocto build system, and using USART1 configure as a hardware flow control RS 232, and RTO interrupt.
and what i found is that CTSIF is not toggling and the proper status are not getting update on CTS from USART SR register. on plug and unplug the usart cable,
i expect when unplug the cable i should get CTSIF event and the status of CTS line.
where the USART1, tx, rx, rts, cts all are set to alternate function and i confirm the linux cflag in stm32-uart.c is true, which the cr3 reg- CTSE and RTSE got set.
1. unplug/ or removing any one of line, i do see still tx is sending the characters/frames,
2. unplug and plug activity checking with or without other device, but i observe the USART cts line is toggling on the oscilloscope.
3. but no interrupt is been observed on stm32_interrupt(irq, *ptr) - stm32-usart.c
Has any one faced this issue on your board and fixed it please do let me know. Thank you.
2024-02-21 2:00 AM
Hello expertise! Could you provide information? Let me know if you need more details.
Thanks!
2024-02-22 10:39 PM
Hello Anyone is there to help me on this issue,
Please give me guidance for this problem.
thanks.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.