2026-03-04 10:58 PM
Hi,
Can I use only M33 core as a standalone controller on stm32mp257 evaluation board without need of linux operating system and DDR
2026-03-05 1:05 AM
This is what we name M33-TD, where Linux on A35 is optional (then you should question choice of STM32MP2 for only M33 core).
Please look to https://wiki.st.com/stm32mpu/wiki/How_to_migrate_STM32CubeMPU_examples_from_A35-TD_flavor_to_M33-TD_flavor
and https://wiki.st.com/stm32mpu/wiki/STM32MP2_boot_chain_overview#STM32MP2_M33-TD_flavor_boot_chain
In our SW deliveries, DDR is assumed mandatory due to limited internal RAM size and our default choice of having M33 TF-M and application code copied from external Flash to DDR instead of XiP (because XiP is limited to Serial-Flash/RAM and not possible on eMMC or SD-Card).
But you could probably build you SW differently (then with limited ST support).
Regards.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.