2026-03-03 3:19 PM - edited 2026-03-03 5:41 PM
I spotted that the documentation and code examples do not match for port pin assignments for LED2 and LED 4.
The user manual manual does not match the schematics:
Code examples do match the schematics, so just a documentation error I think.
EDIT: There is definitely some sort of misalignment here. The Linux device tree (stm32mp215f-dk.dts) puts the blue LED on PZ3. And when controlled on/off or heartbeat through Linux, the blue led labelled LD2 on the dev kit is controlled. So this seems to match the user manual!
gpio-leds {
compatible = "gpio-leds";
led-blue {
function = LED_FUNCTION_HEARTBEAT;
color = <LED_COLOR_ID_BLUE>;
gpios = <&gpioz 3 GPIO_ACTIVE_HIGH>;
linux,default-trigger = "heartbeat";
default-state = "off";
};
};I can only assume the LED labelled LD4 on the dev kit is wired to pin PF10?
2026-03-04 3:07 AM
Hi @ADunc.1 ,
quickly checked, I think there is no mistake, just component numbering (which is automatic I guess) that are not aligned with PCB signal naming (alignment is not mandatory although is create headache).
Regards.
2026-03-04 12:40 PM
@PatrickF Thanks for checking. Yeah, it's not super ideal having them labelled inconsistently, but not the end of the world. Perhaps a note in that table in the user manual would help clarify.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.