2022-05-24 8:15 PM
I loaded my custom built yocto image into my SD card using the STM32CubeProgrammer and the process was completed successfully.
However, when I toggled the boot switches to boot from SD card, I was not able to connect my host computer (a Ubuntu 20.04 desktop PC) to STM32MP1 board via CN11. When I plugged the micro USB cable from my host computer into CN11 on the STM32MP1 board, my host computer did not detect any new USB device. Can you please advise the steps to troubleshoot this?
2022-05-25 5:16 AM
Hi @CTeo.1
CN11 is directly connected to STLINK, so it's behavior is not related to any SD-Card content nor boot switches.
Once connected to a PC, you should see a composite device with a VCP (for UART console) and a debug port.
Does 'lsusb' shows "STMicroelectronics ST-LINK/V2.1" ?
Maybe try on another PC, maybe try also on a windows PC.
Please check https://wiki.st.com/stm32mpu/wiki/PC_prerequisites
Maybe try to update STLINK FW to latest version https://www.st.com/en/development-tools/stsw-link007.html
Regards,
In order to give better visibility on the answered topics, please click on 'Select as Best' on the reply which solved your issue or answered your question. See also 'Best Answers'
2022-05-25 6:09 AM
2022-05-25 6:20 AM
CubeProgrammer make use of USB DFU from DK2 board CN7 (USB Type-C).
STLINK is connected with CN11 (micro-B connector).
You could run the STLINK FW updater, it will display the current FW version before you are asked to update. There is anyway no drawback to update to latest STLINK FW.
Regards.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.