2025-05-06 4:40 AM
I am trying to debug a simple application on the CM4 processor on a STM32MP157D-DK1 development board in engineering mode using Cube IDE Version: 1.18.1
The board is booted from the micro SD card and appears to be powered up and alive with various flashing LEDs. When I try to debug my simple application I get the following error. I have tried many different debug and connection options on the debug configuration but I cannot seem to get past this point. How can I fix this?
Open On-Chip Debugger 0.12.0+dev-00608-gd8ed48fef (2025-02-06-11:17) [https://github.com/STMicroelectronics/OpenOCD]
Licensed under GNU GPL v2
For bug reports, read
http://openocd.org/doc/doxygen/bugs.html
srst_only srst_pulls_trst srst_gates_jtag srst_open_drain connect_deassert_srst
Info : Listening on port 6666 for tcl connections
Info : Listening on port 4444 for telnet connections
Info : connected to stlink-server
Info : stlink-server API v3, version 2.1.1
Info : STLINK V2J46M31 (API v2) VID:PID 0483:3752
Info : Target voltage: 3.257030
Info : clock speed 4000 kHz
Info : stlink_dap_op_connect(connect)
Info : SWD DPIDR 0x6ba02477
Info : stlink_dap_op_connect(connect)
Info : SWD DPIDR 0x6ba02477
Info : [STM32MP157DACx.ap1] Examination succeed
Info : [STM32MP157DACx.cm4] Cortex-M4 r0p1 processor detected
Info : [STM32MP157DACx.cm4] target has 6 breakpoints, 4 watchpoints
Info : [STM32MP157DACx.ap2] Examination succeed
Info : [STM32MP157DACx.axi] Examination succeed
Info : STM32MP157DACx.cpu0: hardware has 6 breakpoints, 4 watchpoints
Info : [STM32MP157DACx.cpu0] Examination succeed
Info : STM32MP157DACx.cpu1: hardware has 6 breakpoints, 4 watchpoints
Info : [STM32MP157DACx.cpu1] Examination succeed
Info : gdb port disabled
Info : gdb port disabled
Info : gdb port disabled
Info : starting gdb server for STM32MP157DACx.cpu0 on 3334
Info : Listening on port 3334 for gdb connections
Info : starting gdb server for STM32MP157DACx.cm4 on 3333
Info : Listening on port 3333 for gdb connections
Info : [STM32MP157DACx.cm4] external reset detected
Info : accepting 'gdb' connection on tcp/3333
Info : Halt timed out, wake up GDB.
Error: timed out while waiting for target halted
Error executing event gdb-attach on target STM32MP157DACx.cm4:
Info : New GDB Connection: 1, Target STM32MP157DACx.cm4, state: reset
Warn : GDB connection 1 on target STM32MP157DACx.cm4 not halted
Error: GDB missing ack(2) - assumed good
Error: GDB missing ack(2) - assumed good
Error: Error on socket 'GDB': WSAGetLastError==10054, message: An existing connection was forcibly closed by the remote host.
.
shutdown command invoked
Info : dropped 'gdb' connection
2025-08-02 6:14 PM
I'm getting the same issue. Anyone find out what the problem is?
2025-08-04 1:12 AM
@MB11 wrote:
I am trying to debug a simple application on the CM4 processor on a STM32MP157D-DK1 development board in engineering mode using Cube IDE Version: 1.18.1
The board is booted from the micro SD card and appears to be powered up and alive with various flashing LEDs.
......
Hi, @MB11
your message contains contradictory information, either you boot from SD-Card or you are in engineering mode.
Please look at https://wiki.st.com/stm32mpu/wiki/STM32CubeIDE#Arm-C2-AE_Cortex-C2-AE-M_debug_on_STM32_MPU_device
Regards.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.