2023-03-08 11:40 PM
Hi all ~
I'm using our custom board with STM32MP157c MPU.
I'm almost done with everything, and finally I'm going to change the u-boot and kernel splash images.
I referred to the link for changing the u-boot splash image and I think it's very simple.
https://community.st.com/s/question/0D53W000011v9OxSAI/custom-uboot-splash-screen
Before customizing the uboot splash as my own,
First, the point I want to check is that the default ST u-boot splash doesn't appear.
Our board uses the Parallel(RGB) display interface and has 1280x800 resolution.
default kernel splash work fine.
Is there anything I need to change in u-boot regarding the RGB interface and resolution?
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.