STM32 MPUs Products and hardware related

Ask questions and find answers on STM32 microprocessors, including hardware, power, DRAM, flashing, interfacing, device tree, and peripherals.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! STM32MP1 OTP word 10 and 11

Hi, I'm trying to leverage the capability of lower words to be programmed once to one bit by bit to implement a sort of "forever growing counter", not sure if there is a proper naming for this.In the lower OTP zone, if I understood correctly, word 10...

Resolved! STM32MP1 DSI voltage level

I would like to clear up some confusion regarding the DSI VIO, the stm32mp157a datasheet mentions "1.2 V I/O for DSI interface" but in the EV1 kit the LCD used (the RK055AHD042-CT, for which it's impossible to find a datasheet for, could that be shar...

arturo182 by Associate II
  • 8610 Views
  • 6 replies
  • 0 kudos

On a linux stm32mp157 system can gpio with pullup or pull-down resistors be configured in user space ? If yes how?

I just spent a day trying to configure a gpio with internal pullup using gpiolib. Could not get it configured. Then spent 2 days with device drivers and device trees, and got it working. Seems insane to me that configuring gpios should be this comple...

Rc.1 by Associate II
  • 6929 Views
  • 6 replies
  • 0 kudos

Cannot load STPMIC1 regulate driver

I have a customized STM32MP157AAD board with STPMIC1E PMIC.STPMIC1E is pre-programmed to have same NVM as 1A version.After power up, the board can download firmware by CubeMX and run uboot from SD card, even partially boot the linux kernel.However, t...

uouox by Associate II
  • 1524 Views
  • 0 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.