2020-07-07 9:36 AM
I follow the instruction of Building the OpenSTLinux distribution to build the distribution image, /etc/version in the image is 20180309123456. Furthermore, the years of most of the directories and files of root filesystem are 2008. If I am correct, it should be the date/time when I built the image.
Why do I ask this? When I tried the built image with the SD card and saw the year of directories and files are 2008, I wondered whether I flashed correct image to the SD card.
2020-07-10 2:14 AM
Hi @MaxPeng ,
I can provide you thorough information from expert how the value in /etc/version is generated:
*************************************************************************************************************************
The date put on /etc/version are get from the git commit from openembedded-core:
REPRODUCIBLE_TIMESTAMP_ROOTFS=`git -C "/mnt/internal_storage/oetest/oe_openstlinux_dunfell/layers/openembedded-core" log -1 --pretty=%ct 2>/dev/null`
sformatted=`date -u -d @${REPRODUCIBLE_TIMESTAMP_ROOTFS} +%4Y%2m%2d%2H%2M%2S`
echo $sformatted > ${IMAGE_ROOTFS}/etc/version
The date issue come from the time reference because the option %ct return a "%ct: committer date, UNIX timestamp".
the UNIX timestamp are not the same as the pc time
*************************************************************************************************************************
To see if you flashed the correct image you can check e.g. the kernel version.
Hope this helps
Milan
2020-07-10 3:45 AM
Hi Milan,
After reading your explanation, I search the recipes and get these:
meta/classes/image.bbclass-653-reproducible_final_image_task () {
meta/classes/image.bbclass-654- if [ "${BUILD_REPRODUCIBLE_BINARIES}" = "1" ]; then
meta/classes/image.bbclass:655: if [ "$REPRODUCIBLE_TIMESTAMP_ROOTFS" = "" ]; then
meta/classes/image.bbclass:656: REPRODUCIBLE_TIMESTAMP_ROOTFS=`git -C "${COREBASE}" log -1 --pretty=%ct 2>/dev/null` || true
meta/classes/image.bbclass:657: if [ "${REPRODUCIBLE_TIMESTAMP_ROOTFS}" = "" ]; then
meta/classes/image.bbclass:658: REPRODUCIBLE_TIMESTAMP_ROOTFS=`stat -c%Y ${@bb.utils.which(d.getVar("BBPATH"), "conf/bitbake.conf")}`
meta/classes/image.bbclass-659- fi
meta/classes/image.bbclass-660- fi
--
meta/classes/reproducible_build_simple.bbclass-6-export PERL_HASH_SEED = "0"
meta/classes/reproducible_build_simple.bbclass-7-export SOURCE_DATE_EPOCH ??= "1520598896"
meta/classes/reproducible_build_simple.bbclass-8-
meta/classes/reproducible_build_simple.bbclass:9:REPRODUCIBLE_TIMESTAMP_ROOTFS ??= "1520598896"
The epoch time 1520598896 equals to March 9, 2018 12:34:56PM -> 20180309123456 stored in /etc/version
The conf/local.conf contains this:
# Setup environment for builds binary reproducibility
INHERIT += "reproducible_build"I understand the purpose of it is to generate "Reproducible Builds". But instead of using meaningless timestamp 20180309123456. Why not set it to a specific date for a release? For example:
# Setup environment for builds binary reproducibility
# GMT: Thursday, July 9, 2020 11:28:10 PM -> 1594337290
BUILD_REPRODUCIBLE_BINARIES = "1"
export SOURCE_DATE_EPOCH = "1594337290"
REPRODUCIBLE_TIMESTAMP_ROOTFS = "1594337290"
INHERIT += "reproducible_build"Thanks!
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.