2020-07-06 1:12 AM
I am trying to use the GPU with an application where using X display is a prerequisite. I have successfully used GPU previously with Qt5 and simple kms applications like kmscube, but cannot get it working with X. Mesa is always used as the renderer with 0% load on GPU. My question is that is this at all supported with the binaries packed in the gcnano repo?
https://github.com/STMicroelectronics/gcnano-binaries
The Yocto recipes point out the following (meta-st-stm32mp/conf/machine/include/gpu_vivante.inc) :
GPU_USERLAND_LIBRARIES_X11 ?= "mesa"
My doubt arises because of the following:
1) In mesa there is no *_dri.so binary available for the particular GPU to support h/w acceleration.
2) If I look for suitable hardware drivers *_drv.so files in xorg, there is no support for Vivante.
I could not find these anywhere in the ST resources as well.
I have tried using "etnaviv" too, but not much luck there.
The last point is that ST wiki doesn't have much documentation on the GPU.
https://wiki.st.com/stm32mpu/wiki/Category:GPU
Is there any way to procure or access them?
P.S: Please excuse me , if some information is missing. If pointed out, I will edit them in. Thanks in advance.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.