2025-10-17 9:27 PM
Hi ST Community,
I’m using the STM32MP257F-DK board and successfully followed this guide:
Modify, rebuild and reload the firmware
Everything worked fine during the initial setup and firmware modification. Now I’m trying to flash a new image to the SD card and connect to the board again, but I’m unable to establish a connection via ST-LINK. Here’s the error I get:
ST-LINK SN : 003E004A3234510636303532
ST-LINK FW : V3J16M8B5S1
Board : STM32MP257F-DK
Voltage : 3.29V
Error: Unable to get core ID
Error: No STM32 target found! If your product embeds Debug Authentication, please perform a discovery using Debug AuthenticationI’ve set the boot switches to the OFF position (boot from UART/USB), and I suspect that during the previous steps, Secure Boot may have been enabled or modified without me realizing it. Could this be preventing me from accessing the board now?
I’ve already tried:
Updating ST-LINK firmware
“Connect under reset” mode
Checking physical connections and voltage
Is there a way to verify or reset the Secure Boot configuration? Or to recover access to the board if Debug Authentication is now required?
Any help or guidance would be greatly appreciated!
Thanks,
Duc Le
Solved! Go to Solution.
2025-10-18 6:13 AM
I fixed it! The issue was with my cable, so I replaced it with a new one and the problem is resolved.
2025-10-18 6:13 AM
I fixed it! The issue was with my cable, so I replaced it with a new one and the problem is resolved.
2025-10-29 8:57 AM
Hello Duc,
I have the same problem, i tried to connect the board with stm32cubeprogrammer and I got the same issue, even if the cable is good, i’m using windows 11, this is the first time I plugged the board with my pc, the board is fresh, is there any steps to do before connecting to stlink v3 programme ?
NB: all switches for boot are 0
best regards
Lmantou
2025-10-30 8:01 AM
Hi @Lmantou,
On the STM3257F-DK, there are two Type-C ports, right? One for power and UART, and the other for connecting to the STLink. Since you mentioned you're experiencing the same issue as I am, I’m guessing you’ve got the cable for power and UART working fine, as you’re able to get the UART log. The issue seems to be with the other port, the one connected to the STLink. Have you double-checked that this connection is secure and working properly?
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.