2023-08-28 2:06 AM
Hello,
I need to synchronize the time between the A7 and M4 cores. While I found some resources on the ST Community that accessing the STGEN timer from the A7 side.
the article is below
So, I tried this on A7 too.
for reading/writing peripheral registers from the A7 core is outlined in STWiki article.
https://wiki.st.com/stm32mpu/wiki/How_to_read_or_write_peripheral_registers
I think accessing /dev/mem offer a same capability. I tried and successfully employed this approach for UART4. However, I failed when it comes to reading the STGENR using this method.
Could someone provide guidance on how I might access the STGEN timer from the A7 core? If there's a more efficient or recommended way to synchronize the time between the A7 and M4 cores, that information would be invaluable as well.
Thank you for your assistance.
2023-08-28 2:20 AM
Hello @MJo.3,
You can check these links :
Hope that helps!
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2023-08-28 7:11 PM
Hello, @Sarra.S
I read the two links. but still, I can't understand how to access the STGENR.
the first link says CNTFRQ register but it isn't listed on manual.
in second one, I guess this part "4 Software frameworks and drivers " would be an answer but it just send me code without any explanations.
So i checked the code and find
```c
mmio_write_32(STGEN_BASE + CNTCVL_OFF, (uint32_t)counter);
mmio_write_32(STGEN_BASE + CNTCVU_OFF, (uint32_t)(counter >> 32));
static inline void mmio_write_32(uintptr_t addr, uint32_t value)
{
*(volatile uint32_t*)addr = value;
}
```
I think it's the same approach.
So, I guess permission is the key.
how to change the permission to read this value in user space?
2023-08-28 7:19 PM
I said it's about permission but STGENR can be accessed in non-secure mode.
Does non-secure mode mean A7 Linux userspace?
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.