2024-11-24 11:53 PM
Hello everyone,
I would like to ask if it is possible to configure the STM32MP157F-DK2 to boot from a USB SSD instead of an SD card. If so, could you please share the steps or documentation?
Thank you in advance!
Best regards,
Symeon Zapsis
Solved! Go to Solution.
2024-11-25 12:26 AM
Hi @symeon
The STM32MP157F-DK2 always need to do low level boot from SD-Card (other boot interface such as Serial-NOR, Serial-NAND, eMMC or SLC-NAND are not available on this boarD).
The STM32MP1 does not have any way to boot from USB device such as external drive.
Only option is to put TF-A and uBoot on SD-card which will load the kernel from an USB drive.
I'm not expert and I don't know how this is easy or complex to do and if there is bootleneck (e.g. having USB host driver in uBoot).
Regards.
2024-11-25 12:26 AM
Hi @symeon
The STM32MP157F-DK2 always need to do low level boot from SD-Card (other boot interface such as Serial-NOR, Serial-NAND, eMMC or SLC-NAND are not available on this boarD).
The STM32MP1 does not have any way to boot from USB device such as external drive.
Only option is to put TF-A and uBoot on SD-card which will load the kernel from an USB drive.
I'm not expert and I don't know how this is easy or complex to do and if there is bootleneck (e.g. having USB host driver in uBoot).
Regards.
2024-11-25 3:25 AM
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.