2024-11-22 4:36 AM
I installed the distribution package using the stm32mp257f-ev board, but eth1 is visible but eth2 is missing. How do I activate both end0 and end1 in yocto.
2024-11-24 6:38 PM
I can't see the network drive even if I run it according to the address below.
https://wiki.st.com/stm32mpu/wiki/X-LINUX-TSNSWCH_Expansion_Package
2024-11-24 9:36 PM
watch -n1 deptp_tool --get-current-dataset
Every 1.0s: deptp_tool --get-current-dataset stm32mp2: Mon Nov 25 05:35:26 2024
ERROR: ptp_management_local.c:154 ptp_management_connect_local: Failed to connec
t to '/var/run/deptp'
ERROR: io.c:469 ptp_management_tool_connect: Failed to initialize transport
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.