2025-05-01 7:42 AM
I have a new STM32MP157D-DK1. I have booted the board using the enclosed SD card and all appears to be working. The green LED next to CN6 is on, blue LED8 starts flashing a few seconds after power on. One of the block of 4 red LEDs next to the ST-LINK connector is flashing. I have connected the ST-LINK CN11 to a USB port on my Windows 11 laptop. I was assuming that the ST-LINK would be detected by Windows and would appear in the list of devices. However, I see nothing at all. No ST-LINK, no virtual COM ports. I have tried different power supplies for the board, different USB cables for the ST-LINK and different USB ports on the laptop.
Is there something else I need to do to see the ST-LINK or does this indicate the board might have a fault?
My aim was to run a very simple program on the CM4 processor using Cube IDE but so far all it says is No ST-LINK detected. I have various other STM32 dev boards and the ST-LINK and COM ports show up just fine for all of those.
Solved! Go to Solution.
2025-05-02 1:17 PM
Turns out it was a faulty USB cable. In fact, several faulty cables. Went through at least three before I found one that worked.
2025-05-02 1:17 PM
Turns out it was a faulty USB cable. In fact, several faulty cables. Went through at least three before I found one that worked.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.