2020-11-09 2:40 AM
Is it possible to boot over UART on the STM32MP157C-DK2?
I set the BOOT pins as following:
BOOT0 - OFF
BOOT1 - OFF
I am using the FT232 UART-USB Adapter and have connected the following pins:
Here is the CubeProgrammer command and its output:
´´´
$ STM32_Programmer_CLI -c port=/dev/ttyUSB0
-------------------------------------------------------------------
STM32CubeProgrammer v2.5.0
-------------------------------------------------------------------
Serial Port /dev/ttyUSB0 is successfully opened.
Port configuration: parity = even, baudrate = 115200, data-bit = 8,
stop-bit = 1,0, flow-control = off
Timeout error occured while waiting for acknowledgement.
Timeout error occured while waiting for acknowledgement.
Error: Activating device: KO. Please, verify the boot mode configuration and check the serial port configuration. Reset your device then try again...
´´´
Am I doing something wrong?
Regards,
Aleksandar
2020-11-12 12:24 AM
Hi Patrick,
I havent added a pull-up, Ill do it today and check the results. So basically the ROM cannot detect that USART3 TX is activated? And adding a pull-up on it could fix i?
Regards
2020-11-12 12:36 AM
This is not related to the ROM, but rather on your UART<->USB cable behavior in case TX is Hi-Z.
In order to avoid any interaction on user board, each UART_TX are kept Hi-Z until the 0x7F is received on one valid RX pin. Then the related TX is enabled (i.e. driven high) and the ROM send acknowledge. Your cable might detect the transition from Hi-Z to high as a character (or an end of 'break' state) and might not correctly manage the first data.
But even without pull-up, you should see some activity on the TX line if you put an analyzer/oscilloscope. Are you sure of your cable wirings (signals and power) ?
2020-11-12 12:57 AM
The wiring is okay, Ive checked it many times. I measured the data on the TX Pin (CN2 PIN 10 GPIO15), the 0x7F is detected, but no activity on the RX pin (CN2 PIN 8 GPIO14). Ill measure everything today again (with and without the pull-up) and write the results here.
Regards
2020-11-12 11:20 AM
Hi Patrick,
we have changed the USB-UART Adapter and it should work soon. However, I am still wondering about the flashing. You mentioned we cannot flash over UART at the moment and we need some uBoot changes to avoid conflict with uBoot Console. Could you point me to someone who could help me with the necessary changes in U-Boot?
Regards
2020-11-17 9:24 AM
Hi @Community member
Please give it a try with a freshly release DV2.1 (see wiki) , taking care to enable usart3 in Uboot DT ( disabled by default)
Olivier
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.