2020-07-30 7:53 AM
I would like to provide power from PI connector. How to avoid error blocking message at the start of the boot that report:
***********************************************
* ERROR USB TYPE-C connection in unattached mode *
* Check that USB TYPE-C cable is correctly plugged *
* Current too low, use a 3A power supply! *
***********************************************
Solved! Go to Solution.
2020-07-30 8:15 AM
Hi,
We did not recommend using Arduino or GPIO expansion connectors to feed 5V to the DK1/DK2 board. the 5V_VIN power routing is not be guaranteed for 3A.
Furthermore, you will probably need to remove Q1 and Q2 to disconnect Type-C VBUS.
If you still want to do that at your own risk, you could remove the warning by choosing one of this 'hack':
Regards.
2020-07-30 8:15 AM
Hi,
We did not recommend using Arduino or GPIO expansion connectors to feed 5V to the DK1/DK2 board. the 5V_VIN power routing is not be guaranteed for 3A.
Furthermore, you will probably need to remove Q1 and Q2 to disconnect Type-C VBUS.
If you still want to do that at your own risk, you could remove the warning by choosing one of this 'hack':
Regards.
2020-07-30 9:59 AM
Thanks for the quickly answer.
We would like to use external power only to make a prototype, then we are ready to design our carrier board with the SOM.
For HW solution its clear.
For SW solution, I found on U-Boot source the file stm32mp1.c with function named "board_check_usb_power(void)". What need I do? Force to "return 0" on line 402?
2020-07-31 5:48 AM
Looking at the code, I propose to replace on line 462
/* with 125ms interval, led will blink for 17.02 years ....*/
nb_blink = U32_MAX;by something like
/* with 125ms interval, led will blink for 17.02 years ....*/
nb_blink = 4;So, the message is still there, but after 4 red led blinks (instead of 2^32 blinks !), the boot will continue.
2020-11-03 3:28 AM
I too want to connect a external power supply. My application is fairly low-power, so it should be OK with the DK2. I tried the HW solution 10K from CC1 to VBUS, but somehow I did not get rid of the message. How do I apply the SW solution to the distrubution package? Do i need to make a .patch file or a .bbappend?
EDIT: HW solution works now, 10K should be connected to 5v_IN, not VBUS.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.